Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General USB UART Driver Problems
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 374 subscribers
  • Views 1805 views
  • Users 0 members are here
Related

USB UART Driver Problems

e14 Contributor
e14 Contributor over 11 years ago

Dear Sir or Madam,

I have several problems to connect my Zynq-7000 EPP 7Z020 ZedBoard via USB. I have downloaded the Cypress USB-UART driver here https://secure.cypress.com/?mpn=CY7C64225-28PVXC and followed the following instructions to install it: http://zedboard.org/sites/default/files/documentations/CY7C64225_Setup_Guide_1_3.pdf

The installation seemed to work fine but after I attached the ZedBoard I did not have the "CypressUsbConsoleWindowsDriver" list inside my Device Manager. The COM-Port is displayed but as "USB Serial Port (COM4)" and not as "Cypress Serial (COM4)". Apart from that, when I enter the advanced settings of the COM-Port I don't have the possibilty to enable "Port Persist". When I try to connect to the board using the program "Tera Term" it does not react and I do not get any answer inside the terminal.

I hope you can help me since I do not have any idea what I could have done wrong. I tried the whole procedure with two different PCs, one running Windows 7 and the other Windows 8.1.

Thank you very much in advance!

Yours sincerely,
Alexander T. Lange, German Aerospace Center (DLR)

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Alex,

    It just looks like that the COM-PORT representation has changed. Kindly look under device manager, specific COM Port->Driver, if you find Cypress seems like it might be working. Press BTN7 to reset and try visualizing on the tera term again with the specified baud rate.
    Worked for me!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi Alex,

    It just looks like that the COM-PORT representation has changed. Kindly look under device manager, specific COM Port->Driver, if you find Cypress seems like it might be working. Press BTN7 to reset and try visualizing on the tera term again with the specified baud rate.
    Worked for me!