Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed won't turn on
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 372 subscribers
  • Views 1051 views
  • Users 0 members are here
Related

MicroZed won't turn on

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I have a MicroZed Z7020 board marked "BD-Z7MB-7Z020-G- Rev-F01". I'm following along with the avnet "Developing Zynq Software with
Xilinx SDK" training, and i'm at the part in Lab 5 where I connect the board. I try to power it with a USB cable, and no LEDs come on.

I also tried to troubleshoot it and read the MicroZed getting started guide ( http://zedboard.org/sites/default/files/documentations/MicroZed_GettingStarted_v1_1.pdf )
as well as the Hardware Users Guide ( http://zedboard.org/sites/default/files/documentations/MicroZed_HW_UG_v1_6.pdf ).

I have Jumpers JP1, JP2, and JP3 all connected up high away from the edge of the board.

I don't have a JTAG cable yet, but I was just trying to power it on via USB @ J2.

Powering it via a USB 3.0 port doesn't turn on LEDs, nor does connected it to a 5V/1A phone charger.

Am I supposed to do something else first, or should the LEDs at least come on?

Thanks!,

Richard Collins

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    If you purchased the version with C01 in the part number, then your board won't work in standalone mode. Do you have the part number from your invoice? Do you have a carrier to plug it into?

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    I do not have the invoice, as it was given (or at least loaned) to me as-is. No extra parts, no SD-Card, no cables. Just the board. I don't think I can ask about an invoice either, since I was told it was purchased a while ago, but the guy never had the time to use it.

    Is there a way to find out by inspecting the board?

    Thanks,

    - Rich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    I do not have the invoice, as it was given (or at least loaned) to me as-is. No extra parts, no SD-Card, no cables. Just the board. I don't think I can ask about an invoice either, since I was told it was purchased a while ago, but the guy never had the time to use it.

    Is there a way to find out by inspecting the board?

    Thanks,

    - Rich