Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed won't turn on
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 372 subscribers
  • Views 1061 views
  • Users 0 members are here
Related

MicroZed won't turn on

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I have a MicroZed Z7020 board marked "BD-Z7MB-7Z020-G- Rev-F01". I'm following along with the avnet "Developing Zynq Software with
Xilinx SDK" training, and i'm at the part in Lab 5 where I connect the board. I try to power it with a USB cable, and no LEDs come on.

I also tried to troubleshoot it and read the MicroZed getting started guide ( http://zedboard.org/sites/default/files/documentations/MicroZed_GettingStarted_v1_1.pdf )
as well as the Hardware Users Guide ( http://zedboard.org/sites/default/files/documentations/MicroZed_HW_UG_v1_6.pdf ).

I have Jumpers JP1, JP2, and JP3 all connected up high away from the edge of the board.

I don't have a JTAG cable yet, but I was just trying to power it on via USB @ J2.

Powering it via a USB 3.0 port doesn't turn on LEDs, nor does connected it to a 5V/1A phone charger.

Am I supposed to do something else first, or should the LEDs at least come on?

Thanks!,

Richard Collins

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    If you purchased the version with C01 in the part number, then your board won't work in standalone mode. Do you have the part number from your invoice? Do you have a carrier to plug it into?

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    On the box I received it in, it has a printed label that says "AES-Z7MB-7Z010-SOM-G", except that the 7Z010 is crossed out, and 7Z020 is written in, and it is, indeed the 7Z020, as seen on the chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    That pat number indicates a 'standard' 7020 MicroZed. Just to confirm, there should be a sticker on the back of the MicroZed board with :BD-Z7MB-7Z020-G-" followed by a "REV-" with the board revision number. 

     

    If that is the case, even though the BOOT jumpers are set to JTAG mode, you should still see a green D5 LED light to indicate that the power supplies came up correctly. If D5 does not light when the micro-USB cable is connected to a suitable USB power source on J2 it looks like you have a problem with your board.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Correct. The sticker on the back is "BD-Z7MB-7Z020-G-" followed by a space and then "REV-F01".

    Multiple power supplies (computer and cell phone chargers of different amp ratings) later, and no green light. No LEDs turn on at all.

    Is there a way to get a replacement, or will I have to buy a new one?

    Thanks,

    Rich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    If it is within the one year warranty period you can request an RMA from the source you bought the board from.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    ok,

    Thank you for your help.

    - Rich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    ok,

    Thank you for your help.

    - Rich