Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Problem booting Linux.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 374 subscribers
  • Views 1609 views
  • Users 0 members are here
Related

Problem booting Linux.

e14 Contributor
e14 Contributor over 12 years ago

I've gone through Chapter 6 of CTT (ug873) to integrate AXI CDMA with Zynq PS HP slave port. I'm aware that the guide is for ZC702 which has 1GB memory whereas Zedboard has 512MB memory.

I've successfully implemented the standalone application (baremetal application of section 6.2) and it works fine without any problem. But I'm having problem with the Linux OS example shown in section 6.3.

I generated FSBL and BOOT.bin by using SDK. Also, I used devicetree.dtb, u-boot.elf (to generate BOOT.bin), zImage and ramdisk8M.image.gz that come with ug873 user guide.

I then copied all the above files to the SD card and turned on Zedboard. But, there wasn't anything happened. There wasn't a single character printed on Tera Term. I guess Linux didn't boot at all.

My question is - do I have to change the devicetree.dtb in this case?

Thank you very much.   

  • Sign in to reply
  • Cancel
  • 100prathima
    0 100prathima over 12 years ago

    Hi,
    I am facing issues using AXI CDMA on bare metal application. Could you please help me out?
    I have followed all the steps in chapter 6 of UG873.
    Further, I have changed HP0 and HP2 addresses to 0x1FA00000 and 0x1FB00000, which is within zedboard's DDR range.
    I am running the example file-
    C:Xilinx14.6ISE_DSEDKswXilinxProcessorIPLibdriversaxicdma_v2_03_aexamplesxaxicdma_example_simple_poll.c
    But if fails to trigger the DMA.
    Please tell me what am I missing.
    Which example are you running? can you share it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Have you tried with the CDMA app comes with the  user guide?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100prathima
    0 100prathima over 12 years ago

    Where can I download it?
    can you pls post the link here?
    I saw this link in the CTT:
    Download ug873_design_files.zip from-
    http://www.xilinx.com/support/documentation/zynq-7000_user_guides.htm
    But I didn't see any zip file there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100prathima
    0 100prathima over 12 years ago

    Thanks kbkien! I got it downloaded. The application works.
    Is there any way to modify this to transfer data from PL to DDR?
    Has anyone tried it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You will need to change devicetree.dtb to match the differences between the ZC702 and the ZedBoard.

     

    The folks at Xillybus have an excellent tutorial on the devicetree. http://xillybus.com/tutorials/device-tree-zynq-1

     

    There is a previous post on the forum that might be helpful as well: http://zedboard.org/content/dts-syntax-and-interrupts-pl-under-linux

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100prathima
    0 100prathima over 12 years ago in reply to e14 Contributor

    Thanks for the quick response Gary!
    Both the links you mentioned is for linux OS.
    But I need to transfer data from PL to PS in a baremetal app.
    Please guide me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to 100prathima

    The reply was to the original post, which was about devicetree.dtb and booting from Linux.

     

    If you want to ask questions on a different topic it is best to start a new thread.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks, Gary. I'll take a look on the links provided. I found out that Xilinx actually has device tree generator ( http://xilinx.wikidot.com/device-tree-generator ). Can this be used in this case?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks for all the suggestions. I tried to generate the device tree by Xilinx device tree generator. Then, I converted the dts file to dtb file by ./scripts/dtc/dtc.

    Now, there are something shown on my Tera Term but there are all funny words like:

    )u00E4u00FBexu00C8u00C83 K      +%
            Hu00E8
    u00BDu00E61u00FBu00E1u00CCKe  u00C4     )u00E9u00A0HW
                         ?H^u00CAzhHu00BAJ

    I did make sure the baud rate of my Tera Term configured to 115200. These are my device tree dts file looks like:


    /dts-v1/;
    / {
    t#address-cells = <1>;
    t#size-cells = <1>;
    tcompatible = "xlnx,zynq-zc770", "xlnx,zynq-7000";
    tmodel = "Xilinx Zynq";
    taliases {
    ttethernet0 = &ps7_ethernet_0;
    ttserial0 = &ps7_uart_1;
    t} ;
    tchosen {
    tt/*bootargs = "console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=1";*/
    ttbootargs = "console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M earlyprintk rootwait devtmpfs.mount=1";
    ttlinux,stdout-path = "/axi@0/serial@e0001000";
    t} ;
    tcpus {
    tt#address-cells = <1>;
    tt#cpus = <0x2>;
    tt#size-cells = <0>;
    ttps7_cortexa9_0: cpu@0 {
    tttcompatible = "xlnx,ps7-cortexa9-1.00.a";
    tttd-cache-line-size = <0x20>;
    tttd-cache-size = <0x8000>;
    tttdevice_type = "cpu";
    ttti-cache-line-size = <0x20>;
    ttti-cache-size = <0x8000>;
    tttmodel = "ps7_cortexa9,1.00.a";
    tttreg = <0>;
    tttxlnx,cpu-1x-clk-freq-hz = <0x69f6bcb>;
    tttxlnx,cpu-clk-freq-hz = <0x27bc86bf>;
    tt} ;
    ttps7_cortexa9_1: cpu@1 {
    tttcompatible = "xlnx,ps7-cortexa9-1.00.a";
    tttd-cache-line-size = <0x20>;
    tttd-cache-size = <0x8000>;
    tttdevice_type = "cpu";
    ttti-cache-line-size = <0x20>;
    ttti-cache-size = <0x8000>;
    tttmodel = "ps7_cortexa9,1.00.a";
    tttreg = <1>;
    tttxlnx,cpu-1x-clk-freq-hz = <0x69f6bcb>;
    tttxlnx,cpu-clk-freq-hz = <0x27bc86bf>;
    tt} ;
    t} ;
    tpmu {
    ttcompatible = "arm,cortex-a9-pmu";
    ttinterrupt-parent = <&ps7_scugic_0>;
    ttinterrupts = < 0 5 4 0 6 4 >;
    ttreg = < 0xf8891000 0x1000 0xf8893000 0x1000 >;
    t} ;
    tps7_ddr_0: memory@0 {
    ttdevice_type = "memory";
    ttreg = < 0x0 0x20000000 >;
    t} ;
    tps7_axi_interconnect_0: amba@0 {
    tt#address-cells = <1>;
    tt#size-cells = <1>;
    ttcompatible = "xlnx,ps7-axi-interconnect-1.00.a", "simple-bus";
    ttranges ;
    ttaxi_cdma_0: axicdma@80200000 {
    ttt#address-cells = <1>;
    ttt#size-cells = <1>;
    tttcompatible = "xlnx,axi-cdma";
    tttranges = < 0x80200000 0x80200000 0x10000 >;
    tttreg = < 0x80200000 0x10000 >;
    tttxlnx,include-sg = <0x0>;
    tttdma-channel@80200000 {
    ttttcompatible = "xlnx,axi-cdma-channel";
    ttttinterrupt-parent = <&ps7_scugic_0>;
    ttttinterrupts = < 0 59 4 >;
    ttttxlnx,datawidth = <0x400>;
    ttttxlnx,include-dre = <0x0>;
    ttttxlnx,lite-mode = <0x0>;
    ttttxlnx,max-burst-len = <0x100>;
    ttt} ;
    tt} ;
    ttps7_ddrc_0: ps7-ddrc@f8006000 {
    tttcompatible = "xlnx,ps7-ddrc-1.00.a", "xlnx,ps7-ddrc";
    tttreg = < 0xf8006000 0x1000 >;
    tttxlnx,has-ecc = <0x0>;
    tt} ;
    ttps7_dev_cfg_0: ps7-dev-cfg@f8007000 {
    tttcompatible = "xlnx,ps7-dev-cfg-1.00.a";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 8 4 >;
    tttreg = < 0xf8007000 0x1000 >;
    tt} ;
    ttps7_dma_s: ps7-dma@f8003000 {
    ttt#dma-cells = <1>;
    ttt#dma-channels = <8>;
    ttt#dma-requests = <4>;
    tttarm,primecell-periphid = <0x41330>;
    tttcompatible = "xlnx,ps7-dma-1.00.a", "arm,primecell", "arm,pl330";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 13 4 0 14 4 0 15 4 0 16 4 0 17 4 0 40 4 0 41 4 0 42 4 0 43 4 >;
    tttreg = < 0xf8003000 0x1000 >;
    tt} ;
    ttps7_ethernet_0: ps7-ethernet@e000b000 {
    ttt#address-cells = <1>;
    ttt#size-cells = <0>;
    tttcompatible = "xlnx,ps7-ethernet-1.00.a";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 22 4 >;
    tttlocal-mac-address = [ 00 0a 35 00 00 00 ];
    tttphy-handle = <&phy0>;
    tttphy-mode = "rgmii-id";
    tttreg = < 0xe000b000 0x1000 >;
    tttxlnx,enet-clk-freq-hz = <0x7735940>;
    tttxlnx,enet-slcr-1000mbps-div0 = <0x8>;
    tttxlnx,enet-slcr-1000mbps-div1 = <0x1>;
    tttxlnx,enet-slcr-100mbps-div0 = <0x8>;
    tttxlnx,enet-slcr-100mbps-div1 = <0x5>;
    tttxlnx,enet-slcr-10mbps-div0 = <0x8>;
    tttxlnx,enet-slcr-10mbps-div1 = <0x32>;
    tttxlnx,eth-mode = <0x1>;
    tttxlnx,has-mdio = <0x1>;
    tttxlnx,ptp-enet-clock = <111111115>;
    tttmdio {
    tttt#address-cells = <1>;
    tttt#size-cells = <0>;
    ttttphy0: phy@7 {
    tttttcompatible = "marvell,88e1116r";
    tttttdevice_type = "ethernet-phy";
    tttttreg = <7>;
    tttt} ;
    ttt} ;
    tt} ;
    ttps7_gpio_0: ps7-gpio@e000a000 {
    ttt#gpio-cells = <2>;
    tttcompatible = "xlnx,ps7-gpio-1.00.a";
    tttemio-gpio-width = <1>;
    tttgpio-controller ;
    tttgpio-mask-high = <0xc0000>;
    tttgpio-mask-low = <0xfe81>;
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 20 4 >;
    tttreg = < 0xe000a000 0x1000 >;
    tt} ;
    ttps7_iop_bus_config_0: ps7-iop-bus-config@e0200000 {
    tttcompatible = "xlnx,ps7-iop-bus-config-1.00.a";
    tttreg = < 0xe0200000 0x1000 >;
    tt} ;
    ttps7_pl310_0: ps7-pl310@f8f02000 {
    tttarm,data-latency = < 3 2 2 >;
    tttarm,tag-latency = < 2 2 2 >;
    tttcache-level = < 2 >;
    tttcache-unified ;
    tttcompatible = "xlnx,ps7-pl310-1.00.a", "arm,pl310-cache";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 2 4 >;
    tttreg = < 0xf8f02000 0x1000 >;
    tt} ;
    ttps7_qspi_0: ps7-qspi@e000d000 {
    tttbus-num = <0>;
    tttcompatible = "xlnx,ps7-qspi-1.00.a";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 19 4 >;
    tttis-dual = <0>;
    tttnum-chip-select = <1>;
    tttreg = < 0xe000d000 0x1000 >;
    tttspeed-hz = <200000000>;
    tttxlnx,fb-clk = <0x1>;
    tttxlnx,qspi-clk-freq-hz = <0xbebc200>;
    tttxlnx,qspi-mode = <0x0>;
    tt} ;
    ttps7_qspi_linear_0: ps7-qspi-linear@fc000000 {
    tttcompatible = "xlnx,ps7-qspi-linear-1.00.a";
    tttreg = < 0xfc000000 0x1000000 >;
    tttxlnx,qspi-clk-freq-hz = <0xe4e1c0>;
    tt} ;
    ttps7_ram_0: ps7-ram@0 {
    tttcompatible = "xlnx,ps7-ram-1.00.a", "xlnx,ps7-ocm";
    tttreg = < 0xfffc0000 0x40000 >;
    tt} ;
    ttps7_scugic_0: ps7-scugic@f8f01000 {
    ttt#address-cells = < 2 >;
    ttt#interrupt-cells = < 3 >;
    ttt#size-cells = < 1 >;
    tttcompatible = "xlnx,ps7-scugic-1.00.a", "arm,cortex-a9-gic", "arm,gic";
    tttinterrupt-controller ;
    tttlinux,phandle = < 0x1 >;
    tttphandle = < 0x1 >;
    tttreg = < 0xf8f01000 0x1000 0xf8f00100 0x100 >;
    tt} ;
    ttps7_scutimer_0: ps7-scutimer@f8f00600 {
    tttcompatible = "xlnx,ps7-scutimer-1.00.a", "arm,cortex-a9-twd-timer";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 1 13 769 >;
    tttreg = < 0xf8f00600 0x20 >;
    tt} ;
    ttps7_scuwdt_0: ps7-scuwdt@f8f00620 {
    tttcompatible = "xlnx,ps7-scuwdt-1.00.a";
    tttdevice_type = "watchdog";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 1 14 769 >;
    tttreg = < 0xf8f00620 0xe0 >;
    tt} ;
    ttps7_sd_0: ps7-sdio@e0100000 {
    tttclock-frequency = <50000000>;
    tttcompatible = "xlnx,ps7-sdio-1.00.a", "generic-sdhci";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 24 4 >;
    tttreg = < 0xe0100000 0x1000 >;
    tttxlnx,has-cd = <0x1>;
    tttxlnx,has-power = <0x0>;
    tttxlnx,has-wp = <0x1>;
    tttxlnx,sdio-clk-freq-hz = <0x2faf080>;
    tt} ;
    ttps7_slcr_0: ps7-slcr@f8000000 {
    tttcompatible = "xlnx,ps7-slcr-1.00.a", "xlnx,zynq-slcr";
    tttreg = < 0xf8000000 0x1000 >;
    tttclocks {
    tttt#address-cells = <1>;
    tttt#size-cells = <0>;
    ttttarmpll: armpll {
    ttttt#clock-cells = <0>;
    tttttclock-output-names = "armpll";
    tttttclocks = <&ps_clk>;
    tttttcompatible = "xlnx,zynq-pll";
    tttttlockbit = <0>;
    tttttreg = < 0x100 0x110 0x10c >;
    tttt} ;
    ttttddrpll: ddrpll {
    ttttt#clock-cells = <0>;
    tttttclock-output-names = "ddrpll";
    tttttclocks = <&ps_clk>;
    tttttcompatible = "xlnx,zynq-pll";
    tttttlockbit = <1>;
    tttttreg = < 0x104 0x114 0x10c >;
    tttt} ;
    ttttiopll: iopll {
    ttttt#clock-cells = <0>;
    tttttclock-output-names = "iopll";
    tttttclocks = <&ps_clk>;
    tttttcompatible = "xlnx,zynq-pll";
    tttttlockbit = <2>;
    tttttreg = < 0x108 0x118 0x10c >;
    tttt} ;
    ttttps_clk: ps_clk {
    ttttt#clock-cells = <0>;
    tttttclock-frequency = <33333333>;
    tttttclock-output-names = "ps_clk";
    tttttcompatible = "fixed-clock";
    tttt} ;
    ttt} ;
    tt} ;
    ttps7_uart_1: serial@e0001000 {
    tttcompatible = "xlnx,ps7-uart-1.00.a", "xlnx,xuartps";
    tttcurrent-speed = <115200>;
    tttdevice_type = "serial";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 50 4 >;
    tttport-number = <0>;
    tttreg = < 0xe0001000 0x1000 >;
    tttxlnx,has-modem = <0x0>;
    tttxlnx,uart-clk-freq-hz = <0x5f5e100>;
    tt} ;
    ttps7_usb_0: ps7-usb@e0002000 {
    tttcompatible = "xlnx,ps7-usb-1.00.a";
    tttdr_mode = "host";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 21 4 >;
    tttphy_type = "ulpi";
    tttreg = < 0xe0002000 0x1000 >;
    tt} ;
    ttps7_xadc: ps7-xadc@f8007100 {
    tttcompatible = "xlnx,ps7-xadc-1.00.a";
    tttinterrupt-parent = <&ps7_scugic_0>;
    tttinterrupts = < 0 7 4 >;
    tttreg = < 0xf8007100 0x20 >;
    tt} ;
    t} ;
    } ;

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Open up the Zynq configuration in your hardware design and make sure that the UART clock frequency is set to 50 MHz as Uboot is expecting. If it is something other than 50 MHz (like 100 MHz) you will need to change the setting and rebuild your hardware platform, regenerate your FSBL, etc.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>