Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Problem booting Linux.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 374 subscribers
  • Views 1608 views
  • Users 0 members are here
Related

Problem booting Linux.

e14 Contributor
e14 Contributor over 12 years ago

I've gone through Chapter 6 of CTT (ug873) to integrate AXI CDMA with Zynq PS HP slave port. I'm aware that the guide is for ZC702 which has 1GB memory whereas Zedboard has 512MB memory.

I've successfully implemented the standalone application (baremetal application of section 6.2) and it works fine without any problem. But I'm having problem with the Linux OS example shown in section 6.3.

I generated FSBL and BOOT.bin by using SDK. Also, I used devicetree.dtb, u-boot.elf (to generate BOOT.bin), zImage and ramdisk8M.image.gz that come with ug873 user guide.

I then copied all the above files to the SD card and turned on Zedboard. But, there wasn't anything happened. There wasn't a single character printed on Tera Term. I guess Linux didn't boot at all.

My question is - do I have to change the devicetree.dtb in this case?

Thank you very much.   

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks again, Gary. Yes! I checked my hardware configuration and it is set to 100 MHz.

    I tried to edit UART clk on Xilinx Platform System but it is just not editable. I saw some comments online and some people said it has to be configured manually.

    I edited it manually (as per zedboard.org_ps-uart-clocking-configuration ) but it still showing funny words.

    Which file(s) should I edit to change the clock frequency of UART?

    Your help is greatly appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks again, Gary. Yes! I checked my hardware configuration and it is set to 100 MHz.

    I tried to edit UART clk on Xilinx Platform System but it is just not editable. I saw some comments online and some people said it has to be configured manually.

    I edited it manually (as per zedboard.org_ps-uart-clocking-configuration ) but it still showing funny words.

    Which file(s) should I edit to change the clock frequency of UART?

    Your help is greatly appreciated.