Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General opencv example application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 374 subscribers
  • Views 864 views
  • Users 0 members are here
Related

opencv example application

e14 Contributor
e14 Contributor over 9 years ago

Hello,

I'm trying to run the example OpenCV application in the SDK on zedboard. But when I'm trying to run it , there is an error.

error: while loading shared libraries: libavformat.so.54: cannot open shared object file: No such file or directory

By following the below link

https://www.xilinx.com/support/documentation/sw_manuals/xilinx14_7/SDK_Doc/tasks/sdk_t_opencv_template.htm

I use the setenv  LD_LIBRARY_PATH = /usr/lib/opencv and try to run, error is

setenv: not found

Then I've copied the opencv libraries from the sdk's opencv to SD card from SSH terminal, mounted the sd card on to /mnt folder and given the below command in the Run configuration dialog box

export LD_LIBRARY_PATH = /mnt/opencv   then it says

export: : bad variable name

 

Does any one have an idea how to solve this ?

Regards

  • Sign in to reply
  • Cancel
Parents
  • albertabeef
    0 albertabeef over 9 years ago

    You need the opencv libraries on your development PC, as well as on the embedded Zynq platform.

    I would recommend looking at the following Xiinx Base TRD design for more details:

       http://www.wiki.xilinx.com/Zynq+Base+TRD+2015.4

    What tool version are you using ?

    What hardware are you targetting ?

    If you are using ZedBoard, you can also consult the following design, which is a port of the Xilinx Base TRD to ZedBoard.

       ZedBoard + FMC-HDMI-CAM + PYTHON-1300-C Vivado HLS Reference Design, Vivado 2015.4

          http://zedboard.org/sites/default/files/design/FMCHC_PYTHON1300C_HLS_2015_4_02_zedboard.zip 

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • albertabeef
    0 albertabeef over 9 years ago

    You need the opencv libraries on your development PC, as well as on the embedded Zynq platform.

    I would recommend looking at the following Xiinx Base TRD design for more details:

       http://www.wiki.xilinx.com/Zynq+Base+TRD+2015.4

    What tool version are you using ?

    What hardware are you targetting ?

    If you are using ZedBoard, you can also consult the following design, which is a port of the Xilinx Base TRD to ZedBoard.

       ZedBoard + FMC-HDMI-CAM + PYTHON-1300-C Vivado HLS Reference Design, Vivado 2015.4

          http://zedboard.org/sites/default/files/design/FMCHC_PYTHON1300C_HLS_2015_4_02_zedboard.zip 

    Regards,

    Mario.