Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General opencv example application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 374 subscribers
  • Views 860 views
  • Users 0 members are here
Related

opencv example application

e14 Contributor
e14 Contributor over 9 years ago

Hello,

I'm trying to run the example OpenCV application in the SDK on zedboard. But when I'm trying to run it , there is an error.

error: while loading shared libraries: libavformat.so.54: cannot open shared object file: No such file or directory

By following the below link

https://www.xilinx.com/support/documentation/sw_manuals/xilinx14_7/SDK_Doc/tasks/sdk_t_opencv_template.htm

I use the setenv  LD_LIBRARY_PATH = /usr/lib/opencv and try to run, error is

setenv: not found

Then I've copied the opencv libraries from the sdk's opencv to SD card from SSH terminal, mounted the sd card on to /mnt folder and given the below command in the Run configuration dialog box

export LD_LIBRARY_PATH = /mnt/opencv   then it says

export: : bad variable name

 

Does any one have an idea how to solve this ?

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Thanks Alberta for the reply.

    I'm using 2015.2 version.

    And targeting Zedboard.

    From the ug1144 , Pg:62 I tried to add the opencv libraries from SDK folder.

    Now I used 'find' to know if the libraries are included in the newly built petalinux. Including the screenshot below


    image

    When I run,

    error: while loading shared libraries: libavformat.so.54: cannot open shared object file: No such file or directory

    Also I edited the makefile accordingly while adding the libraries. 

    Also I'm looking into the links you've provided and will revert back if there is any progress

    Regards 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Thanks Alberta for the reply.

    I'm using 2015.2 version.

    And targeting Zedboard.

    From the ug1144 , Pg:62 I tried to add the opencv libraries from SDK folder.

    Now I used 'find' to know if the libraries are included in the newly built petalinux. Including the screenshot below


    image

    When I run,

    error: while loading shared libraries: libavformat.so.54: cannot open shared object file: No such file or directory

    Also I edited the makefile accordingly while adding the libraries. 

    Also I'm looking into the links you've provided and will revert back if there is any progress

    Regards