Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General FMC reference design ?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 372 subscribers
  • Views 1293 views
  • Users 0 members are here
Related

FMC reference design ?

e14 Contributor
e14 Contributor over 14 years ago

Does anyone know of a general reference design for a vita57 fmc card for eagle cad?

Having one available here would be great.

Found a design for a fmc  card using sata connectors(not proper sata) here
http://danstrother.com/2010/12/04/fmc-lpc-to-sata-adapter-board/



Thanks


Alex

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    This brings up a great point Alex.  Since the Zedboard is meant for hobbyists, educators and students, and those who many be just starting out in the world of programmable logic, an Eagle Cad library would be a great addition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    This brings up a great point Alex.  Since the Zedboard is meant for hobbyists, educators and students, and those who many be just starting out in the world of programmable logic, an Eagle Cad library would be a great addition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Its not just hobbiests using eagle.

    At work some departments use Altium, others use Eagle. Its a cost thing.

    Eagle is also the only cross platform cad.
    Its the main option if you need cad for linux and mac.

    Would be nice if xilinx supported macs like microchip has done (latest mplabx is available on linux , mac and windows).

    For most embedded systems these days you don't need windows for development and its easier and less problems to use linux with tools like git, svn , eclipse .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I certainly agree that it is not only hobbyiests and students using Eagle Cad - however with the Zed board being targeted to that group of engineers/enthusiasts, it would make sense to have a library to pull from.  The initiative to start this library has already started, and hopefully will be finished soon! (note: not supported by Avnet, Digilent, or Xilinx).

    As for the Mac developers environment for the Xilinx tools: You can always run a VM and run Linux on Mac OS - it is very simple.  As for a roadmap for native support, I will have to look into that.