Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Done LED not on
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 631 views
  • Users 0 members are here
Related

Done LED not on

e14 Contributor
e14 Contributor over 13 years ago

Hello,

recently, I got my zedboards, and I powered it, but both boards DONE led does not show up after 15 seconds.

the Power Good LED is lit on.

When I connect the Platform Cable USB II to the JTAG Port, I get an error Message in iMPACT, that two unknown devices are found, requiring an BSDL file for them.

When I hook up the micro-usb cable to PROG (J17), the Drivers are installed successfully, but Impact complaines about "Error:Impact:2246 A reference voltage has not been detected ..."

Did I get two defect boards?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    The first batch of production boards may not have shipped with the expected board configuration.  There were some last minute changes to the functional test at the CM that affected this.

    The included Quick Start card in the kit is abbreviated and assumes the proper configuration.  Please download the full Getting Start Guide from the Documentation page and follow it.  As described in that guide, you'll need to set several jumpers for SD Boot Mode as well as installing the SD Card.  Then you should see the Linux boot, which does include the DONE LED going high as there is some video IP loaded in the PL.

    Sorry for the confusion.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    The first batch of production boards may not have shipped with the expected board configuration.  There were some last minute changes to the functional test at the CM that affected this.

    The included Quick Start card in the kit is abbreviated and assumes the proper configuration.  Please download the full Getting Start Guide from the Documentation page and follow it.  As described in that guide, you'll need to set several jumpers for SD Boot Mode as well as installing the SD Card.  Then you should see the Linux boot, which does include the DONE LED going high as there is some video IP loaded in the PL.

    Sorry for the confusion.

    Bryan