Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Done LED not on
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 627 views
  • Users 0 members are here
Related

Done LED not on

e14 Contributor
e14 Contributor over 13 years ago

Hello,

recently, I got my zedboards, and I powered it, but both boards DONE led does not show up after 15 seconds.

the Power Good LED is lit on.

When I connect the Platform Cable USB II to the JTAG Port, I get an error Message in iMPACT, that two unknown devices are found, requiring an BSDL file for them.

When I hook up the micro-usb cable to PROG (J17), the Drivers are installed successfully, but Impact complaines about "Error:Impact:2246 A reference voltage has not been detected ..."

Did I get two defect boards?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I tried to connect with an older iMPACT Software.
    I can connect to the JTAG Port now.

    And I got the Linux to boot up correctly. But I had to read the README file on the sd-card to set the jumper correctly. This readme file should be part of the getting started guide and you shold add a note to the zedboard enclosed print "Getting Started Instructions": Please set the jumper according to README file on sd-card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The Title of my last post is wrong. I had Problems with the UART, but then I saw the README file on the sd-card. I forgot to change the title.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    The first batch of production boards may not have shipped with the expected board configuration.  There were some last minute changes to the functional test at the CM that affected this.

    The included Quick Start card in the kit is abbreviated and assumes the proper configuration.  Please download the full Getting Start Guide from the Documentation page and follow it.  As described in that guide, you'll need to set several jumpers for SD Boot Mode as well as installing the SD Card.  Then you should see the Linux boot, which does include the DONE LED going high as there is some video IP loaded in the PL.

    Sorry for the confusion.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Decide to reject that negative attitude, of what is being impacted over the wireless transmissions, or by and large discussion.
    Zyban - http://www.genericviagraus.net/zyban_generic.html