Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SDR Training
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 692 views
  • Users 0 members are here
Related

SDR Training

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I am trying to work on the SDR training using Simulink (the lab 2 hw).  When I navigate to the to the downloaded files, I get a different file name than is provided in the pdf, "commtimrecresample_dsp_start" vs "commtimrecresample_dsp_v23_start."  Also, when I try to simulate the QPSK Generator, I get the following errors:

External Model firv6_3_CModel:firv6_3_cmodel threw std::exception:
An error occurred during HDL compilation. ERROR:HDLCompiler:1206 - "fir_compiler_v6_3_control.vhd" Line 155: Syntax error near '"'

ERROR:HDLCompiler:1206 - "fir_compiler_v6_3_control.vhd" Line 156: Syntax error near '"'

ERROR:HDLCompiler:1206 - "fir_compiler_v6_3_control.vhd" Line 156: Syntax error near '"'

ERROR:HDLCompiler:806 - "fir_compiler_v6_3_control.vhd" Line 155: Syntax error near """.

ERROR:HDLCompiler:806 - "fir_compiler_v6_3_control.vhd" Line 156: Syntax error near """.

ERROR:HDLCompiler:854 - "fir_compiler_v6_3_control.vhd" Line 86: Unit <behavioral> ignored due to previous errors.


Error occurred during "Simulation Initialization".


Reported by:
'commtimrecresample_dsp_start/DFE for Radio Rx/Xilinx 2X Decimation Halfband Filter RX/FIR Compiler 6.3 phase_1'

Any help would be great.

Nathan

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Xilinx Fir Compiler / System Generator 14.4 has issues with R2012b. Consequently, as noted in the documentation, ISE / SysGen 14.3 is used for the Simulink labs. Subsequently, for Xilinx Platform Studio (XPS), you will need 14.1. This is where the development was at when we finalized the SpeedWay labs.

     

    To summarize the tools requirements:

     

    MathWorks MATLAB & Simulink R2012b

       DSP System Toolbox

       Signal Processing Toolbox

       Fixed-Point Toolbox

       Simulink Fixed Point

     

    Xilinx ISE Design Suite 14.3 System Edition (used for lab 2)

    Xilinx ISE Design Suite 14.1 System Edition (used for lab 3)

     

    DSP_1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    @SDR_1

    Thanks for your reply.  I installed 14.3 and everything is working for me now.  I missed that the tutorial was designed using ISE 14.3.  I had used 14.4 for the other Speedway training courses without much of an issue.

    Nathan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    @SDR_1

    Thanks for your reply.  I installed 14.3 and everything is working for me now.  I missed that the tutorial was designed using ISE 14.3.  I had used 14.4 for the other Speedway training courses without much of an issue.

    Nathan