Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General SDR Training
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 692 views
  • Users 0 members are here
Related

SDR Training

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I am trying to work on the SDR training using Simulink (the lab 2 hw).  When I navigate to the to the downloaded files, I get a different file name than is provided in the pdf, "commtimrecresample_dsp_start" vs "commtimrecresample_dsp_v23_start."  Also, when I try to simulate the QPSK Generator, I get the following errors:

External Model firv6_3_CModel:firv6_3_cmodel threw std::exception:
An error occurred during HDL compilation. ERROR:HDLCompiler:1206 - "fir_compiler_v6_3_control.vhd" Line 155: Syntax error near '"'

ERROR:HDLCompiler:1206 - "fir_compiler_v6_3_control.vhd" Line 156: Syntax error near '"'

ERROR:HDLCompiler:1206 - "fir_compiler_v6_3_control.vhd" Line 156: Syntax error near '"'

ERROR:HDLCompiler:806 - "fir_compiler_v6_3_control.vhd" Line 155: Syntax error near """.

ERROR:HDLCompiler:806 - "fir_compiler_v6_3_control.vhd" Line 156: Syntax error near """.

ERROR:HDLCompiler:854 - "fir_compiler_v6_3_control.vhd" Line 86: Unit <behavioral> ignored due to previous errors.


Error occurred during "Simulation Initialization".


Reported by:
'commtimrecresample_dsp_start/DFE for Radio Rx/Xilinx 2X Decimation Halfband Filter RX/FIR Compiler 6.3 phase_1'

Any help would be great.

Nathan

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Good morning, I need help with the generation of the BIN file to the SD Card, I follow the steps of the laboratories. The simulation is perfect, the system generator compiles without problems, make the connection instance of the TX and RX module, I generate the BIN file Zedboard recognize the card over Linux or the board from Analog Devices Radio is live. Could someone give me a hint, follow the link attached my project. Thank you,
    http://www.sendspace.com/file/k13lru

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Good morning, I need help with the generation of the BIN file to the SD Card, I follow the steps of the laboratories. The simulation is perfect, the system generator compiles without problems, make the connection instance of the TX and RX module, I generate the BIN file Zedboard recognize the card over Linux or the board from Analog Devices Radio is live. Could someone give me a hint, follow the link attached my project. Thank you,
    http://www.sendspace.com/file/k13lru