Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General iic Device Id
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 375 subscribers
  • Views 880 views
  • Users 0 members are here
Related

iic Device Id

473srikanth
473srikanth over 10 years ago

Hello friends,

                       i'm working on iicps examples for establishing i2c communication between a zedboard and a sensor(i2c based). In the examples for iic there is a macro IIC_DEVICE_ID. and in the main there is a comment,

/*
* Run the Iic Slave Monitor example, specify the Device ID that is
* generated in xparameters.h.

*/

what is this Device ID macro ??

Thanks in advance. 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello 473srikanth,

    As you have found the instance or 'device id' of the IIC device you are using is defined in the xparameters.h file that was generated as part of your BSP to match your hardware configuration. This device ID is passed to the example code you reference above which, in turn, calls code defined in the xiicps.h file that is in the 'src' directory of the iicps_v3 drivers. Here is a snippet of the coments in the xiicps.h code regarding use of the DeviceID:

    * The XIicPs_Config structure is used by the driver to configure itself. This
    * configuration structure is typically created by the tool-chain based on HW
    * build properties.
    *
    * To support multiple runtime loading and initialization strategies employed by
    * various operating systems, the driver instance can be initialized in the
    * following way:
    *
    *    - XIicPs_LookupConfig(DeviceId) - Use the device identifier to find
    *      the static configuration structure defined in xiicps_g.c. This is
    *      setup by the tools. For some operating systems the config structure
    *      will be initialized by the software and this call is not needed.
     
    You can follow the declaration through the calls in the example code for more details.
     
    -Gary
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello 473srikanth,

    As you have found the instance or 'device id' of the IIC device you are using is defined in the xparameters.h file that was generated as part of your BSP to match your hardware configuration. This device ID is passed to the example code you reference above which, in turn, calls code defined in the xiicps.h file that is in the 'src' directory of the iicps_v3 drivers. Here is a snippet of the coments in the xiicps.h code regarding use of the DeviceID:

    * The XIicPs_Config structure is used by the driver to configure itself. This
    * configuration structure is typically created by the tool-chain based on HW
    * build properties.
    *
    * To support multiple runtime loading and initialization strategies employed by
    * various operating systems, the driver instance can be initialized in the
    * following way:
    *
    *    - XIicPs_LookupConfig(DeviceId) - Use the device identifier to find
    *      the static configuration structure defined in xiicps_g.c. This is
    *      setup by the tools. For some operating systems the config structure
    *      will be initialized by the software and this call is not needed.
     
    You can follow the declaration through the calls in the example code for more details.
     
    -Gary
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer