Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Lab1.1 on SDK 14.5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 372 subscribers
  • Views 312 views
  • Users 0 members are here
Related

Lab1.1 on SDK 14.5

e14 Contributor
e14 Contributor over 13 years ago

Hi,

Has anyone tried to build the Zynq FSBL with the latest Xilinx tools (ISE 14.5)?

I've met several problems already and some I was able to work-around. But I am still not able to have it build.

* In PlanAhead I had to regenerate the bitstream and make sure to also load the implementation. Only then was I able to Export Hardware for SDK including the bitstream.
* Instead of a Xilinx C Project I had to choose a New Application Project in the SDK.
* Then it turns out almost all include directories are missing so I right-clicked src->properties and added the following include directories:
  C:Xilinx14.5ISE_DSEDKswlibbspstandalone_v3_04_asrccortexa9
  C:Xilinx14.5ISE_DSEDKswlibbspstandalone_v3_04_asrccortexa9gcc
  C:Xilinx14.5ISE_DSEDKswlibbspstandalone_v3_04_asrccommon
  C:Xilinx14.5ISE_DSEDKswXilinxProcessorIPLibdriverscommon_v1_00_asrc
  C:Xilinx14.5ISE_DSEDKswXilinxProcessorIPLibdriversdevcfg_v2_02_asrc
  C:Xilinx14.5ISE_DSEDKswXilinxProcessorIPLibdriverswdtps_v1_02_asrc
* You cannot use the (newer) standalone_v3_09_a directory.
* In fsbl.h I replaced include xparameters.h with xparameters_ps.h

But even after all this it still fails to build with a missing definition for XPAR_PS7_WDT_0_WDT_CLK_FREQ_HZ. I cannot find where this symbol should come from.

Can anybody help me? I'm pretty much lost and feel the only solution is to revert to ISE 14.2. That would mean another big download and another long install.

Kind regards,
Maarten

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I've been using 14.5 and can create a boot image. The only thing I can suggest is to insure that PlanAhead is started from the ISE Command Window and that you delete and rebuild the BSP. It took me several tries before I got it right, in the end it came down to:

    1. Launch from ISE command windows
    2. Create a BSP, watch it fail to compile. Delete, then rebuild.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I don't think I understand what you mean. Are you suggesting I should start in ISE (with an ISE project) and open PlanAhead from there (what is the command window?) and then open the SDK from PlanAhead?

    As mentioned I'm trying to redo Lab1.1 from the Avnet course:
    Implementing Linux on the Zynq-7000 SoC
        Open Source Linux
    Development on ZedBoard

    I can delete the BSP, but that doesn't really help because the build fails to compile main.c of the application project. I think it doesn't even get around to the BSP.

    Should I choose to create a New -> C Project instead of a New -> Application Project? It doesn't seem so.

    It looks to me as if Xilinx distributes an old FSBL template with a new and incompatible library.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Ok, I finally found it. When the Project is created it generates an error message, but due to the auto-build option of eclipse (the SDK) it is immediately purged and you get to see the build errors instead.

    Failed to copy from
      C:Xilinx14.2ISE_DSEDKswlibbspstandalone_v3_06_asrc into
       files.vanmierlo.comprojectenVan_Mierlo_IngenieursbureauProjectenVMI-BESZynq_cursusZynq_linuxlab1_1LED_ControllerLED_Controller.sdkSDKSDK_Exportzynq_fsbl_bsp_0ps7_cortexa9_0libsrcstandalone_v3_06_asrc.

    So somehow the SDK decided to replace my mapped driveletter with the underlying serverpath and then was unable to use that path.

    Long story short: Do not try to use your network-drive! So far for automatic backup of your data :(