Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Lab1.1 on SDK 14.5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 372 subscribers
  • Views 315 views
  • Users 0 members are here
Related

Lab1.1 on SDK 14.5

e14 Contributor
e14 Contributor over 13 years ago

Hi,

Has anyone tried to build the Zynq FSBL with the latest Xilinx tools (ISE 14.5)?

I've met several problems already and some I was able to work-around. But I am still not able to have it build.

* In PlanAhead I had to regenerate the bitstream and make sure to also load the implementation. Only then was I able to Export Hardware for SDK including the bitstream.
* Instead of a Xilinx C Project I had to choose a New Application Project in the SDK.
* Then it turns out almost all include directories are missing so I right-clicked src->properties and added the following include directories:
  C:Xilinx14.5ISE_DSEDKswlibbspstandalone_v3_04_asrccortexa9
  C:Xilinx14.5ISE_DSEDKswlibbspstandalone_v3_04_asrccortexa9gcc
  C:Xilinx14.5ISE_DSEDKswlibbspstandalone_v3_04_asrccommon
  C:Xilinx14.5ISE_DSEDKswXilinxProcessorIPLibdriverscommon_v1_00_asrc
  C:Xilinx14.5ISE_DSEDKswXilinxProcessorIPLibdriversdevcfg_v2_02_asrc
  C:Xilinx14.5ISE_DSEDKswXilinxProcessorIPLibdriverswdtps_v1_02_asrc
* You cannot use the (newer) standalone_v3_09_a directory.
* In fsbl.h I replaced include xparameters.h with xparameters_ps.h

But even after all this it still fails to build with a missing definition for XPAR_PS7_WDT_0_WDT_CLK_FREQ_HZ. I cannot find where this symbol should come from.

Can anybody help me? I'm pretty much lost and feel the only solution is to revert to ISE 14.2. That would mean another big download and another long install.

Kind regards,
Maarten

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I've been using 14.5 and can create a boot image. The only thing I can suggest is to insure that PlanAhead is started from the ISE Command Window and that you delete and rebuild the BSP. It took me several tries before I got it right, in the end it came down to:

    1. Launch from ISE command windows
    2. Create a BSP, watch it fail to compile. Delete, then rebuild.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I've been using 14.5 and can create a boot image. The only thing I can suggest is to insure that PlanAhead is started from the ISE Command Window and that you delete and rebuild the BSP. It took me several tries before I got it right, in the end it came down to:

    1. Launch from ISE command windows
    2. Create a BSP, watch it fail to compile. Delete, then rebuild.