Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General PartitionLoadAddr is not in the range
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 860 views
  • Users 0 members are here
Related

PartitionLoadAddr is not in the range

e14 Contributor
e14 Contributor over 12 years ago

I followed the instruction for petalinux and create the linux image and BOOT.BIN

$ petalinux-package --boot --fsbl <FSBL image> --fpga <FPGA bitstream> --uboot

The uart screen output

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>


Xilinx First Stage Boot Loader

Release 14.6/2013.2     May 23 2014-09:08:31

Devcfg driver initialized

Silicon Version 3.1

Boot mode is SD

SD: rc= 0

SD Init Done

Flash Base Address: 0xE0100000

Reboot status register: 0x60600000

Multiboot Register: 0x0000C000

Image Start Address: 0x00000000

Partition Header Offset:0x000009C0

Partition Count: 3

Partition Number: 1

Header Dump

Image Word Len: 0x000F6EC0

Data Word Len: 0x000F6EBF

Partition Word Len:0x000F6EC0

Load Addr: 0x00000000

Exec Addr: 0x00000000

Partition Start: 0x000062C0

Partition Attr: 0x00000020

Partition Checksum Offset: 0x00000000

Section Count: 0x00000001

Checksum: 0xFFD14E8F

Bitstream

Encrypted

In FsblHookBeforeBitstreamDload function

PCAP:StatusReg = 0x40000A30

PCAP:device ready

PCAP:Clear done

Level Shifter Value = 0xA

Devcfg Status register = 0x40000A30

PCAP:Fabric is Initialized done

PCAP register dump:

PCAP CTRL 0xF8007000: 0x4E00E07F

PCAP LOCK 0xF8007004: 0x0000001A

PCAP CONFIG 0xF8007008: 0x00000508

PCAP ISR 0xF800700C: 0x0802000B

PCAP IMR 0xF8007010: 0xFFFFFFFF

PCAP STATUS 0xF8007014: 0x0006DA30

PCAP DMA SRC ADDR 0xF8007018: 0x00100001

PCAP DMA DEST ADDR 0xF800701C: 0xFFFFFFFF

PCAP DMA SRC LEN 0xF8007020: 0x000F6EC0

PCAP DMA DEST LEN 0xF8007024: 0x000F6EBF

PCAP ROM SHADOW CTRL 0xF8007028: 0xFFFFFFFF

PCAP MBOOT 0xF800702C: 0x0000C000

PCAP SW ID 0xF8007030: 0x00000000

PCAP UNLOCK 0xF8007034: 0x757BDF0D

PCAP MCTRL 0xF8007080: 0x30800100

DMA Done !

FPGA Done !

In FsblHookAfterBitstreamDload function

Partition Number: 2

Header Dump

Image Word Len: 0x0000EFC3

Data Word Len: 0x0000EFC3

Partition Word Len:0x0000EFC3

Load Addr: 0x3FC00000

Exec Addr: 0x3FC00000

Partition Start: 0x000FD180

Partition Attr: 0x00000010

Partition Checksum Offset: 0x00000000

Section Count: 0x00000001

Checksum: 0x806D5CC5

Application

PartionLoadAddr 3FC00000 DDR_START_ADDR 00100000 DDR_END_ADDR 1FFFFFFF

INVALID_LOAD_ADDRESS_FAIL

FSBL Status = 0xA00F

This Boot Mode Doesn't Support Fallback

In FsblHookFallback function

<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<


The output

PartionLoadAddr 3FC00000 DDR_START_ADDR 00100000 DDR_END_ADDR 1FFFFFFF

indicates that load address is not in valid range.

My question is that DDR_START_ADDR and DDR_END_ADDR are defined in xparameters.h which was created by Xilinx SDK but how does petalinux determine the PartitionLoadAddr.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Gary,

    My xparameters.h file says

    /* Definitions for peripheral PS7_DDR_0 */

    #define XPAR_PS7_DDR_0_S_AXI_BASEADDR 0x00100000

    #define XPAR_PS7_DDR_0_S_AXI_HIGHADDR 0x1FFFFFFF

    so it seems correct.

    I am using manual ug980-petalinux-board-bringup.pdf and when creating application project, I choose zed_hw_platform(predefined)as the hardware platform. I do get the error when I execute the command

    shashi@Zynq002:~/projects/zedboard01/zed_prj_bsp$ petalinux-config --get-hw-description -p ../zedlnx

    INFO: Checking component...

    INFO: Getting hardware description...

    INFO: Using MSS file /home/shashi/projects/zedboard01/zed_prj_bsp/system.mss and XML file /home/shashi/projects/zedboard01/zed_prj_bsp/../zed_hw_platform/system.xml

    INFO: Copy autoconfig for PetaLinux project: /home/shashi/projects/zedboard01/zedlnx

    ERROR: Only single-cpu PetaLinux OS type supported.

    ERROR: Failed to sync up hardware description!

    But I proceeded further anyway.

    Instead of using petalinux-package to create BOOT.BIN as I had done in my original mail, I decided to use bootgen with the appropriate load and start address


    the_ROM_image:

    {
        [bootloader]./zed_boot/Debug/zed_boot.elf

        ./zedlnx/images/linux/system.bit

        [load = 0x101000, startup = 0x101000]./zedlnx/images/linux/u-boot.elf

    }

    Note that this works correctly with windows ce but not with linux.



    Now, I don't get the error but the system hang, and do not proceed to execute the second stage boot loader


    Handoff Address: 0x00101000

    In FsblHookBeforeHandoff function

    SUCCESSFUL_HANDOFF

    FSBL Status = 0x1


    Looking at the code, I can see that the start address is not correct.

    So, I am asking how do sync the hw-description from my bsp to my project.

    How can I get hands on Avnet Petalinux Speedway lab ?

    Also, Is there a manual which can help me build the boot image directly from Xilinx source tree.



    Thanks



    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Gary,

    My xparameters.h file says

    /* Definitions for peripheral PS7_DDR_0 */

    #define XPAR_PS7_DDR_0_S_AXI_BASEADDR 0x00100000

    #define XPAR_PS7_DDR_0_S_AXI_HIGHADDR 0x1FFFFFFF

    so it seems correct.

    I am using manual ug980-petalinux-board-bringup.pdf and when creating application project, I choose zed_hw_platform(predefined)as the hardware platform. I do get the error when I execute the command

    shashi@Zynq002:~/projects/zedboard01/zed_prj_bsp$ petalinux-config --get-hw-description -p ../zedlnx

    INFO: Checking component...

    INFO: Getting hardware description...

    INFO: Using MSS file /home/shashi/projects/zedboard01/zed_prj_bsp/system.mss and XML file /home/shashi/projects/zedboard01/zed_prj_bsp/../zed_hw_platform/system.xml

    INFO: Copy autoconfig for PetaLinux project: /home/shashi/projects/zedboard01/zedlnx

    ERROR: Only single-cpu PetaLinux OS type supported.

    ERROR: Failed to sync up hardware description!

    But I proceeded further anyway.

    Instead of using petalinux-package to create BOOT.BIN as I had done in my original mail, I decided to use bootgen with the appropriate load and start address


    the_ROM_image:

    {
        [bootloader]./zed_boot/Debug/zed_boot.elf

        ./zedlnx/images/linux/system.bit

        [load = 0x101000, startup = 0x101000]./zedlnx/images/linux/u-boot.elf

    }

    Note that this works correctly with windows ce but not with linux.



    Now, I don't get the error but the system hang, and do not proceed to execute the second stage boot loader


    Handoff Address: 0x00101000

    In FsblHookBeforeHandoff function

    SUCCESSFUL_HANDOFF

    FSBL Status = 0x1


    Looking at the code, I can see that the start address is not correct.

    So, I am asking how do sync the hw-description from my bsp to my project.

    How can I get hands on Avnet Petalinux Speedway lab ?

    Also, Is there a manual which can help me build the boot image directly from Xilinx source tree.



    Thanks