Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General PartitionLoadAddr is not in the range
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 858 views
  • Users 0 members are here
Related

PartitionLoadAddr is not in the range

e14 Contributor
e14 Contributor over 12 years ago

I followed the instruction for petalinux and create the linux image and BOOT.BIN

$ petalinux-package --boot --fsbl <FSBL image> --fpga <FPGA bitstream> --uboot

The uart screen output

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>


Xilinx First Stage Boot Loader

Release 14.6/2013.2     May 23 2014-09:08:31

Devcfg driver initialized

Silicon Version 3.1

Boot mode is SD

SD: rc= 0

SD Init Done

Flash Base Address: 0xE0100000

Reboot status register: 0x60600000

Multiboot Register: 0x0000C000

Image Start Address: 0x00000000

Partition Header Offset:0x000009C0

Partition Count: 3

Partition Number: 1

Header Dump

Image Word Len: 0x000F6EC0

Data Word Len: 0x000F6EBF

Partition Word Len:0x000F6EC0

Load Addr: 0x00000000

Exec Addr: 0x00000000

Partition Start: 0x000062C0

Partition Attr: 0x00000020

Partition Checksum Offset: 0x00000000

Section Count: 0x00000001

Checksum: 0xFFD14E8F

Bitstream

Encrypted

In FsblHookBeforeBitstreamDload function

PCAP:StatusReg = 0x40000A30

PCAP:device ready

PCAP:Clear done

Level Shifter Value = 0xA

Devcfg Status register = 0x40000A30

PCAP:Fabric is Initialized done

PCAP register dump:

PCAP CTRL 0xF8007000: 0x4E00E07F

PCAP LOCK 0xF8007004: 0x0000001A

PCAP CONFIG 0xF8007008: 0x00000508

PCAP ISR 0xF800700C: 0x0802000B

PCAP IMR 0xF8007010: 0xFFFFFFFF

PCAP STATUS 0xF8007014: 0x0006DA30

PCAP DMA SRC ADDR 0xF8007018: 0x00100001

PCAP DMA DEST ADDR 0xF800701C: 0xFFFFFFFF

PCAP DMA SRC LEN 0xF8007020: 0x000F6EC0

PCAP DMA DEST LEN 0xF8007024: 0x000F6EBF

PCAP ROM SHADOW CTRL 0xF8007028: 0xFFFFFFFF

PCAP MBOOT 0xF800702C: 0x0000C000

PCAP SW ID 0xF8007030: 0x00000000

PCAP UNLOCK 0xF8007034: 0x757BDF0D

PCAP MCTRL 0xF8007080: 0x30800100

DMA Done !

FPGA Done !

In FsblHookAfterBitstreamDload function

Partition Number: 2

Header Dump

Image Word Len: 0x0000EFC3

Data Word Len: 0x0000EFC3

Partition Word Len:0x0000EFC3

Load Addr: 0x3FC00000

Exec Addr: 0x3FC00000

Partition Start: 0x000FD180

Partition Attr: 0x00000010

Partition Checksum Offset: 0x00000000

Section Count: 0x00000001

Checksum: 0x806D5CC5

Application

PartionLoadAddr 3FC00000 DDR_START_ADDR 00100000 DDR_END_ADDR 1FFFFFFF

INVALID_LOAD_ADDRESS_FAIL

FSBL Status = 0xA00F

This Boot Mode Doesn't Support Fallback

In FsblHookFallback function

<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<


The output

PartionLoadAddr 3FC00000 DDR_START_ADDR 00100000 DDR_END_ADDR 1FFFFFFF

indicates that load address is not in valid range.

My question is that DDR_START_ADDR and DDR_END_ADDR are defined in xparameters.h which was created by Xilinx SDK but how does petalinux determine the PartitionLoadAddr.

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Xilinx ZC702 board and the MicroZed each have 1 Gig of DDR memory which is assigned an address range of 00100000 to 3FFFFFFF. The ZedBoard only has half as much DDR memory and has an address range of 00100000 to 1FFFFFFF.  It looks like the hardware you generated (for a Zedboard?) does not match the Petalinux you generated or copied.

     

    What instructions did you follow to generate your linux image and boot.bin? Were you following the Avnet Petalinux Speedway lab instructions or something else?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Xilinx ZC702 board and the MicroZed each have 1 Gig of DDR memory which is assigned an address range of 00100000 to 3FFFFFFF. The ZedBoard only has half as much DDR memory and has an address range of 00100000 to 1FFFFFFF.  It looks like the hardware you generated (for a Zedboard?) does not match the Petalinux you generated or copied.

     

    What instructions did you follow to generate your linux image and boot.bin? Were you following the Avnet Petalinux Speedway lab instructions or something else?

     

    -Gary