Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General When reading UART0, strange singals will keep sending into it
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 1499 views
  • Users 0 members are here
Related

When reading UART0, strange singals will keep sending into it

e14 Contributor
e14 Contributor over 9 years ago

Hello everyone, 

I have encountered a strange problem on the UART. When I am reading UART0 from linux using "cat /dev/ttyPS1" or a test app, strange singals will keep sending into the RX port of the UART, why??

Details:

I am using picozed 7015 with petalinux 16.2. UART1 is binding with the console which is functional. UART0 is binding to a GPS module through EMIO. RX and TX of UART0 are pulled up using vivado user constrain.

Using "cat /dev/ttyPS1", I can get continuous messages :

"$GNTXT,01,01,01,NMEA unknown msg*46

$GNTXT,01,01,01,NMEA unknown msg*46"
Suggesting that input cmd is wrong.
Then I use a multimeter to check the RX port when the "cat /dev/ttyPS1" is running, and the voltage of RX port is continuously change.
If I only send something to the RX port of UART1, the GPS module can recv my cmd.
 
Am I missing something ? I have googled but got nothing.. Thanks..
 
 
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello wujingband,

    Take a look at this post https://forum.u-blox.com/index.php?qa=1031&qa_1=gptxt-nmea-unknown-msg-meaning

    Go through the two possible solutions to your problem and please report back.

    Thansk,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hi Josh,

    Thanks for your reply!  Problem is solved by trying the solutions in the post.

    It seems that the tty device will echo input characters in default. This can be un-configured by 

    "struct termios options; 

    options.c_lflag  &= ~ECHO

    ..."

    How stupid I am to neglect this simple configuration.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer