Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Xilinx Linux Build
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 706 views
  • Users 0 members are here
Related

Xilinx Linux Build

e14 Contributor
e14 Contributor over 12 years ago

Good afternoon,

I am using a ZedBoard and i want to build the bootloader files (boot.bin, uimage, etc). I already built several versions (v14.5,v14.7) and with that versions i had always problems with ethernet communication and no access to SDCard. I am following the steps provided by wiki.xilinx.com. My questions is what version is the recommended for ZedBoard and what kind of mistake can i be doing?
I am using ISE 14.5 in windows 7 and Sourcery CodeBench cross toolchain which is xilinx-2011.09-50-arm-xilinx-linux-gnueabi.

Thanks.

Greetings,
Davide Guimaru00E3es

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 12 years ago

    Hi Davide,

    Are you using your own custom hardware platform that you created for ZedBoard or are you using the boot.bin provided with the Xilinx Official Linux release for ZedBoard?

    If you are using your own custom hardware platform, have you enabled the Timer 0 peripheral?  I built a new hardware platform in 14.5 PlanAhead using the ZedBoard board definition and applied the ZedBoard preset template to the Zynq Configurator in XPS.  For these settings Timer 0 is enabled by default and connected to EMIO.

    After building the hardware project and exporting to SDK, building the FSBL from the SDK template, I was able to create a new boot image with the new FSBL, new bitstream, and U-Boot elf provided in the Xilinx Official 14.5 Linux release and it appears to boot the same as the hardware platform configuration provided in the boot.bin which comes with the Xilinx Official 14.5 Linux release archive.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 12 years ago

    Hi Davide,

    Are you using your own custom hardware platform that you created for ZedBoard or are you using the boot.bin provided with the Xilinx Official Linux release for ZedBoard?

    If you are using your own custom hardware platform, have you enabled the Timer 0 peripheral?  I built a new hardware platform in 14.5 PlanAhead using the ZedBoard board definition and applied the ZedBoard preset template to the Zynq Configurator in XPS.  For these settings Timer 0 is enabled by default and connected to EMIO.

    After building the hardware project and exporting to SDK, building the FSBL from the SDK template, I was able to create a new boot image with the new FSBL, new bitstream, and U-Boot elf provided in the Xilinx Official 14.5 Linux release and it appears to boot the same as the hardware platform configuration provided in the boot.bin which comes with the Xilinx Official 14.5 Linux release archive.

    Regards,

    -Kevin