Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Xilinx Linux Build
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 702 views
  • Users 0 members are here
Related

Xilinx Linux Build

e14 Contributor
e14 Contributor over 12 years ago

Good afternoon,

I am using a ZedBoard and i want to build the bootloader files (boot.bin, uimage, etc). I already built several versions (v14.5,v14.7) and with that versions i had always problems with ethernet communication and no access to SDCard. I am following the steps provided by wiki.xilinx.com. My questions is what version is the recommended for ZedBoard and what kind of mistake can i be doing?
I am using ISE 14.5 in windows 7 and Sourcery CodeBench cross toolchain which is xilinx-2011.09-50-arm-xilinx-linux-gnueabi.

Thanks.

Greetings,
Davide Guimaru00E3es

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Kevin,

    Thanks for reply.

    I already did that and i got an error: "timer clock input not found".
    I built the u-boot and linux kernel. After that i ran the boot gen that generated the boot.bin. After i passed the files boot.bin, uImage and the other files i used the pre-compiled files (uramdisk.image and devicetree.dtb) to sd card.
    When i booted the files the zedboard gave me a kernel panic saying that there is no timer clock.

    Greetings,
    Davide

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Kevin,

    Thanks for reply.

    I already did that and i got an error: "timer clock input not found".
    I built the u-boot and linux kernel. After that i ran the boot gen that generated the boot.bin. After i passed the files boot.bin, uImage and the other files i used the pre-compiled files (uramdisk.image and devicetree.dtb) to sd card.
    When i booted the files the zedboard gave me a kernel panic saying that there is no timer clock.

    Greetings,
    Davide