Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Xilinx Linux Build
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 706 views
  • Users 0 members are here
Related

Xilinx Linux Build

e14 Contributor
e14 Contributor over 12 years ago

Good afternoon,

I am using a ZedBoard and i want to build the bootloader files (boot.bin, uimage, etc). I already built several versions (v14.5,v14.7) and with that versions i had always problems with ethernet communication and no access to SDCard. I am following the steps provided by wiki.xilinx.com. My questions is what version is the recommended for ZedBoard and what kind of mistake can i be doing?
I am using ISE 14.5 in windows 7 and Sourcery CodeBench cross toolchain which is xilinx-2011.09-50-arm-xilinx-linux-gnueabi.

Thanks.

Greetings,
Davide Guimaru00E3es

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Kevin,

    I built my owm custom hardware platform and i didn't enabled any timer. I don't need to use it.

    I want use my own u-boot.elf and uImage instead of the files provided in the Xilinx Official 14.5 Linux, to compile files and to configure the kernel.

    I followed the tutorial provided in http://www.wiki.xilinx.com. It is necessary any kind of patch to compile u-boot or linux kernel for zedboard?

    Greetings,
    Davide

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Kevin,

    I built my owm custom hardware platform and i didn't enabled any timer. I don't need to use it.

    I want use my own u-boot.elf and uImage instead of the files provided in the Xilinx Official 14.5 Linux, to compile files and to configure the kernel.

    I followed the tutorial provided in http://www.wiki.xilinx.com. It is necessary any kind of patch to compile u-boot or linux kernel for zedboard?

    Greetings,
    Davide