Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Lab 05 - "undefined reference to 'main'"
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 2187 views
  • Users 0 members are here
Related

Lab 05 - "undefined reference to 'main'"

e14 Contributor
e14 Contributor over 12 years ago

Hello,

Been having this problem for a little while now. I'm currently going through lab 5 of the tutorial and right after I make the main.c file I get these two errors which I can't resolve:

make:***[src/main.o] Error 1   LED_Dimmer
undefined reference to 'main'  xil-crt0.S

Other background is that I recently switched from 14.7 to 14.6 so that I could receive better support from the class that I'm taking right now.

Any ideas on what I could do to fix this?

Regards,
Keyur

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you are trying to start with the 'solution' for Lab 4 from the Intro to Zynq zip file the problem is that the BSP you are using was created by a much earlier version of the Xilinx ISE tools and will need to be updated. I tried generating a new BSP when making the LED_Dimmer application and that corrected the errors that you are seeing.

     

    However there are probably going to be other differences so it would be best to start the tutorial from the start in PlanAhead 14.6 if that is the tool suite you plan to use.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gaurav_acad
    0 gaurav_acad over 12 years ago

    what i did is since BSP was showing this error file , i did right click on it and run clean project.

    i hope it will help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    if you don't have run clean project option you can only change on src file of the BSP and save. It worked for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Click on the board support package and run "Regenerate BSP Sources" worked for me. This happened after I cut and paste a project. I also had to run "Clean Project" on the new project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RahulSoni
    0 RahulSoni over 4 years ago in reply to e14 Contributor

    what change did you make in the BSP file?