Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General initial booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Subscribers 374 subscribers
  • Views 2183 views
  • Users 0 members are here
  • mini-module
  • minimodule
  • zynq
  • mini-module_plus
Related

initial booting

sungyung_lim
sungyung_lim over 10 years ago

We purchased a MMP with zynq 7z100.
Since we followed the simple instruction,
we found that the initial serial connection didn't work.
We used sd card-based booting with factory-installed linux image. Is there any known defect on instruction or linux image? And is there any useful information on it?

Thank you for your consideration in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello S.Y.

     

    We have a Vivado 2014.2 Petalinux Software Reference Design and BSP available on the Zynq MMP Reference Designs and Tutorials page:

     

    http://zedboard.org/support/design/3006/26

     

    The Ethernet connection could be several things. Does the software running on your Zynq MMP board us DHCP or some other method to obtain an IP address or do you set a static IP address? Is the IP address set on the same subnet as your router. Does it conflict with another device on your router with the same IP address?

     

    I have also see this problem when wireless ethernet is enabled on the host PC

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi Gary,
    I have found that my development board will not boot(Config FPGA ( Blue Led)/uboot on serial port and then boot linux kernel) when SW5 is set to 00110 ( SD Card ).
    However, when I choose the QSPI boot SW5 00010, The fpga configs, and I get a serial port console and uboot spits out.  Which is great, but from QSPI and not the SD card.
    However the QSPI boot, fails to boot a linux image.
    rather, just complains about no "sf" command.
    I then use the serial port connection to uboot, to run sdboot and Linux starts booting from the SD card.
    However, it hangs after led-brightness spits out on the serial port.

    So, are the instructions just less than optimal ?
    If so is there new text ?
    Also are the images on the SD Card that came with it old or for another device ?

    Where should I go from here ?  Download latest petalinux ?  I currently have ZMMP_7045_PetaLinux_PL2015_2   Should I go to the latest ?
    Also, is there a support number to contact and ask a couple questions ?
    My email address is aweissman AT acacia-inc.com

    Thanks in advance for any help you can provide


    Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi Gary,
    I have found that my development board will not boot(Config FPGA ( Blue Led)/uboot on serial port and then boot linux kernel) when SW5 is set to 00110 ( SD Card ).
    However, when I choose the QSPI boot SW5 00010, The fpga configs, and I get a serial port console and uboot spits out.  Which is great, but from QSPI and not the SD card.
    However the QSPI boot, fails to boot a linux image.
    rather, just complains about no "sf" command.
    I then use the serial port connection to uboot, to run sdboot and Linux starts booting from the SD card.
    However, it hangs after led-brightness spits out on the serial port.

    So, are the instructions just less than optimal ?
    If so is there new text ?
    Also are the images on the SD Card that came with it old or for another device ?

    Where should I go from here ?  Download latest petalinux ?  I currently have ZMMP_7045_PetaLinux_PL2015_2   Should I go to the latest ?
    Also, is there a support number to contact and ask a couple questions ?
    My email address is aweissman AT acacia-inc.com

    Thanks in advance for any help you can provide


    Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hello Adrian,

     

    This is the best venue for support. I will work on getting an MMP board and see if we can duplicate your issue.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Great, I look forward to hearing from you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Hi Gary,
    Please send me your contact information
    aweissman AT acacia-inc.com

    Cheers,
    Adrian