Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General initial booting
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Subscribers 374 subscribers
  • Views 2182 views
  • Users 0 members are here
  • mini-module
  • minimodule
  • zynq
  • mini-module_plus
Related

initial booting

sungyung_lim
sungyung_lim over 10 years ago

We purchased a MMP with zynq 7z100.
Since we followed the simple instruction,
we found that the initial serial connection didn't work.
We used sd card-based booting with factory-installed linux image. Is there any known defect on instruction or linux image? And is there any useful information on it?

Thank you for your consideration in advance.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Adrian,

     

    A colleague of mine was able to get an MMP board and was able to verify the issue you observed with the QSPI Flash load. It looks like we have a problem with the pre-loaded QSPI image and will work on that. Thanks for alerting us to the problem.

     

    I am not sure exactly what you are seeing with the Out of Box SD Card image. If you push SW10 the LED brightness application should exit and return to the Linux prompt. You can download the Out of Box SD card image, along with documentation and directions on the LED Brightness demo application from the MMP Reference Designs /Tutorials page here:

     

    http://zedboard.org/support/design/3006/26

     

    We also verified that the image available with the MMP compressed PetaLinux BSP, which you can also download from the same MMP Reference Designs page, works correctly. This image is more up to date than the Out of Box SD Card Linux image and you may want to start with that. The compressed BSP image you download is basically a zip file of a zip file, so use WinZip or similar program to extract twice.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks, I will download this new image and give it a try.
    I really appreciate the help !!!

    Adrian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    Thanks, I will download this new image and give it a try.
    I really appreciate the help !!!

    Adrian