Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Question about Lab 6 of Introduction to Zynq
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 520 views
  • Users 0 members are here
Related

Question about Lab 6 of Introduction to Zynq

e14 Contributor
e14 Contributor over 13 years ago

Hi,

I'm following the "Introduction to Zynq" training.
So far so good.

In lab 6 (Adding Interrupts from PL) I get stuck.
On page 4, step 11, the task is:
"Click in the Port connection area for GPIO2_IO_I, which will bring up a dialog."

But that never happens.
RMB gives, No Connection, Make Connection or Make External.
Double clicking gives the "configure dialog" pop-up.

How do I get to the screen that the is shown in the PDF?

I'm using the 14.2 version, provided with the board.

Rgds,
Technicolor

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    I have found XPS to be very temperamental with port connections, sometimes the only way to connect ports is to go into the MHS file and do it by hand.  One way which normally works is to select all the ports you want to connect using ctrl + LMB, then right-click and you should have a "Connect Ports..." option.  I have rarely seen that dialog box come up, whichever version of the tools I was using.

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi

    I have found XPS to be very temperamental with port connections, sometimes the only way to connect ports is to go into the MHS file and do it by hand.  One way which normally works is to select all the ports you want to connect using ctrl + LMB, then right-click and you should have a "Connect Ports..." option.  I have rarely seen that dialog box come up, whichever version of the tools I was using.

    Matthew