Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Where find SDR Training labs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 375 subscribers
  • Views 1291 views
  • Users 0 members are here
Related

Where find SDR Training labs

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I'm searching information about the SDR-Kit and SDR-II Kit. Before I buy a Board, I want to know how to start with it. I have read here about SDR Training with different labs. Where can I find it? Have someboda other Sources for Information?

Thanks

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hey,

    acutally i have the Problem, that the BOOT.bin from the Beacon-Frame-RX example doesn't work with the FMCOMMS2-EZB and zedboard. I replaced the BOOT-file on the SD-Card, but it seems that the FMSCOMMS2-Board doesn't get found by the Linux..

    Do you have any recommendation?

    Greetings
    Jan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hey,

    acutally i have the Problem, that the BOOT.bin from the Beacon-Frame-RX example doesn't work with the FMCOMMS2-EZB and zedboard. I replaced the BOOT-file on the SD-Card, but it seems that the FMSCOMMS2-Board doesn't get found by the Linux..

    Do you have any recommendation?

    Greetings
    Jan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    In Addtion:

    input: Fujitsu Siemens Computers GmbH FSC KBPC PX  as /devices/amba.1/e0002000.u                                                                                                                     sb/zynq-ehci.0/usb1/1-1/1-1.2/1-1.2:1.0/input/input1
    ad9361 spi32766.0: ad9361_dig_tune: Tuning RX FAILED!
    hid-generic 0003:0BF8:100C.0002: input,hidraw1: USB HID v1.10 Keyboard [Fujitsu                                                                                                                      Siemens Computers GmbH FSC KBPC PX ] on usb-zynq-ehci.0-1.2/input0
    input: Fujitsu Siemens Computers GmbH FSC KBPC PX  as /devices/amba.1/e0002000.u                                                                                                                     sb/zynq-ehci.0/usb1/1-1/1-1.2/1-1.2:1.1/input/input2
    hid-generic 0003:0BF8:100C.0003: input,hidraw2: USB HID v1.10 Device [Fujitsu Si                                                                                                                     emens Computers GmbH FSC KBPC PX ] on usb-zynq-ehci.0-1.2/input1
    ad9361 spi32766.0: ad9361_dig_tune: Tuning TX FAILED!
    cf_axi_adc: probe of 79020000.cf-ad9361-lpc failed with error -5
    drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    ALSA device list:
      #0: HDMI monitor
      #1: ZED ADAU1761
    random: nonblocking pool is initialized
    EXT4-fs (mmcblk0p2): 2 orphan inodes deleted
    EXT4-fs (mmcblk0p2): recovery complete
    EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    VFS: Mounted root (ext4 filesystem) on device 179:2.
    Freeing unused kernel memory: 180K (c0557000 - c0584000)
    u2592nit: ureadahead main process (754) terminated with status 5
    Last login: Thu Jan  1 00:00:13 UTC 1970 on tty1
    * Starting IIO Server Daemon iiod                                       [ OK ]
    Welcome to Linaro 12.11 (GNU/Linux 3.13.0-68980-gbcc97b8 armv7l)

    * Documentation:  https://wiki.linaro.org/

    root@linaro-ubuntu-desktop:~#

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • frestuc
    0 frestuc over 8 years ago in reply to e14 Contributor

    Hi all,

    The download links are not working (broken) could you fix them? Thanks!

    Otherwise, can anybody upload these files somewhere so we can download them?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • noamlevine
    0 noamlevine over 8 years ago in reply to frestuc

    Avnet is no longer supporting PicoZed SDR.

    You can also find the examples on the MathWorks site: 

    Examples are listed at https://www.mathworks.com/hardware-support/zynq-sdr.html

    Some short-form tutorial videos are also available:

    •   Tool Setup and Radio I/O
    •   HW/SW Codesign

    In addition, MathWorks offers a formal training class on Zynq-based SDR.