Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ZedBoard doesn't answer after loading a custom bitstream
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 374 subscribers
  • Views 597 views
  • Users 0 members are here
Related

ZedBoard doesn't answer after loading a custom bitstream

jkopp
jkopp over 9 years ago

Hello,


I am using Matlab Simulink, the "Communications System Toolbox Support Package for Xilinx Zynq-Based Radio" and the HDL Workflow Advisor to create HDL-Code and generate a custom bitstream to program the FPGA. Then I load the bitstream onto the board over Ethernet with Matlab. My hardware is the Zedboard and the RF FMC card AD9364.

 

Now, the problem is the following: Sometimes when I generate a bitstream and load it onto the board, it stops responding. When Matlab then tries to start a connection, it fails and reports an "incompatibe radio" and suggests that the SD card image loaded on the board wouldn't be compatible with the Matlab/Simulink version. The wierd thing is however, that at other times when I repeat the whole workflow, it is successful with the exact same Simulink model!

 

My guess is that the Anti-Virus software and/or the firewall is the problem. But wouldn't that result in more consistent behavior?

 

Can you help me? Is this a common issue (I guess not, as I couldn't find anything) or can you guess what the cause for this is?

 

Thank you very much.
Johannes Kopp

  • Sign in to reply
  • Cancel
Parents
  • jkopp
    0 jkopp over 9 years ago

    Hello Matt,

    thanks for the answer. The problem still occurred after I explicitly allowed Matlab's data traffic within the firewall settings. However, I've been working with a completely deactivated firewall since Friday and didn't have any more issues to this point. I would like to find a way to keep the rest of the firewall active though.

     

    I actually didn't run anything on the ARM yet, I was only programming the FPGA.

     

    Thank you for your help,
    Johannes

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jkopp
    0 jkopp over 9 years ago

    Hello Matt,

    thanks for the answer. The problem still occurred after I explicitly allowed Matlab's data traffic within the firewall settings. However, I've been working with a completely deactivated firewall since Friday and didn't have any more issues to this point. I would like to find a way to keep the rest of the firewall active though.

     

    I actually didn't run anything on the ARM yet, I was only programming the FPGA.

     

    Thank you for your help,
    Johannes