Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Unstable
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 487 views
  • Users 0 members are here
Related

Unstable

e14 Contributor
e14 Contributor over 13 years ago

I am going through the getting started guide with my new ZedBoard and find some instability.

It started when I plugged in a 100BT ethernet.

The serial connection (using tera term then later PuTTY) would lock up.  I have to unplug the USB from the Windows 7 computer and replug, then reset the comm session to get going again.

Also, the ZB reboots spontaneously.  Fairly often. 

I unplugged the ethernet and was able to play for about an hour and a half until I plugged back in and things went bad again within about three minutes.

I haven't made any changes to the image yet.

Any suggestions?

Thanks,
Greg

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Is it possible that the Ethernet cord is putting pressure on the board in a way that is causing the board to bend?

    It is rather unlikely that the Ethernet connection on the Zedboard is effecting the COM state on your Windows-7 machine.  However it may be possible that the board is bending and thus interrupting USB traffic which then causes Windows to reject the USB device.

    Try changing your setup a bit and have all the wires lay flat, and not pull on the board.

    I have been using my board a significant amount with various different configurations, and I have not seen this operation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    No undue stresses.

    I also notice that the failures stopped when I switched to to SSH and stopped using the serial port.  When I started using the serial port again (with ethernet still attached) it crashed within a minute.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Odd.  It certainly points to the UART/Ethernet port pairing being the root of the problem.

    Are you able to continue to use SSH for the time being until I can look into this more?

    A few additional questions:

    Are you using USB-OTG?
    Are you using the cables that came with the Zedboard?
    When you say the board crashes, is it completely unresponsive?  Or just via the UART port?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I can use SSH, so it isn't life threatening.

    I am configured as USB OTG.
    I am using the supplied USB cables.

    Sometimes the PuTTY or teraterm session locks such that I need to pull the USB, reinsert, then reset the terminal session.  In this case, the SSH session still works.

    Sometimes the board reboots spontaneously.  I suppose it might be helpful in this case if I were using a persistent 'image' in case something is logged?