Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Xilinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 520 views
  • Users 0 members are here
Related

Xilinux

deaxman
deaxman over 13 years ago

I am a little confused about what version of linux is on the board by default.  From what I can tell xilinux should have dev/xillybus_32 for communication with IO which is what I want.  The default does not have this however.  When I go to the documentation referenced on http://xillybus.com/xillinux at the bottom it just talks about installing xillybus not creating a xilinux operating system.  What is the difference between xillybus and xilinux and how can I replace the default linux with xilinux?  Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    Let's get things in order, then.

    The Zedboard arrives with a SD card containing a basic Linux distribution, which supports a small set of commands by virtue of a piece of software called Busybox. There is no Xillybus support on that, and it has nothing to do with Xillinux.

    Xillinux is a fullblown graphical Linux distribution based upon Ubuntu 12.04, and it includes the Xillybus IP core and driver plus a few other things. The procedure for setting up Xillinux does indeed involve implementing the PL part. Once the system is up and running, you may add your application logic to the ISE project that you've previously implemented. So the somewhat tedious procedure for setting up Xillinux gives you the development environment ready to go.

    The Linux filesystem is available for download as an SD image (see section 3.7 in the docs).

    The two things to download appear at the bottom of the page you gave a link to. The instructions for installing Xillinux are at http://xillybus.com/downloads/doc/xillybus_getting_started_zynq.pdf

    I hope this made things clearer.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,

    Let's get things in order, then.

    The Zedboard arrives with a SD card containing a basic Linux distribution, which supports a small set of commands by virtue of a piece of software called Busybox. There is no Xillybus support on that, and it has nothing to do with Xillinux.

    Xillinux is a fullblown graphical Linux distribution based upon Ubuntu 12.04, and it includes the Xillybus IP core and driver plus a few other things. The procedure for setting up Xillinux does indeed involve implementing the PL part. Once the system is up and running, you may add your application logic to the ISE project that you've previously implemented. So the somewhat tedious procedure for setting up Xillinux gives you the development environment ready to go.

    The Linux filesystem is available for download as an SD image (see section 3.7 in the docs).

    The two things to download appear at the bottom of the page you gave a link to. The instructions for installing Xillinux are at http://xillybus.com/downloads/doc/xillybus_getting_started_zynq.pdf

    I hope this made things clearer.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • deaxman
    0 deaxman over 13 years ago in reply to e14 Contributor

    Thanks!  This helped a ton!