Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Maximum clock speed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 1570 views
  • Users 0 members are here
Related

Maximum clock speed

e14 Contributor
e14 Contributor over 13 years ago


I'm interested to know if the on-board 100 MHz clock can be changed for a faster one, and what will be the maximum speed we can operate on the Zedboard.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    daviddlc,

    The clock can be increased using the PLL's on the Zynq device.

    Here is the clocking users guide for the 7-series device:

    http://www.xilinx.com/support/documentation/user_guides/ug472_7Series_Clocking.pdf

    Chapter 3, on page 61 begins the description and functionality of the Mixed-Mode Clock Management (MMCM) and Phase Lock Loop (PLL).

    As far as the maximum frequency, that is greatly dependent on the quality of your code.  In the case of 'perfect code' the maximum is several hundred megahertz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 13 years ago

    The 100 MHz clock (IC17) on ZedBoard is a Fox Electronics 767-100-136.  That family of oscillators goes up to 250 MHz.  If you are good at soldering, then you could swap out the oscillator.  However, using the internal clocking resources to synthesize a clock like TimDuffy suggests is probably the best way to go.  You'll be responsible for making sure your design in PL can meet timing at whatever clock rate you decide.

     

    The datasheets for all the Fox oscillators used on ZedBoard are now posted on the Docs page under Hardware Guide.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deaxman
    0 deaxman over 12 years ago in reply to e14 Contributor

    What do you mean by "quality".  If there is a lot of code and a lot of resources are used but it is high quality (as in very efficent) does that mean that it is better than something that uses less resources but is less efficent?  Or is this maximum clock speed entirely dependant on the amount of resources used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    A9 CPU: 866 MHz is max freq for most Zynq versions, 1GHz for the largest versions. www.xilinx.com/publications/prod_mktg/zynq7000/Zynq-7000-combined-product-table.pdf