Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Maximum clock speed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 1573 views
  • Users 0 members are here
Related

Maximum clock speed

e14 Contributor
e14 Contributor over 13 years ago


I'm interested to know if the on-board 100 MHz clock can be changed for a faster one, and what will be the maximum speed we can operate on the Zedboard.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    daviddlc,

    The clock can be increased using the PLL's on the Zynq device.

    Here is the clocking users guide for the 7-series device:

    http://www.xilinx.com/support/documentation/user_guides/ug472_7Series_Clocking.pdf

    Chapter 3, on page 61 begins the description and functionality of the Mixed-Mode Clock Management (MMCM) and Phase Lock Loop (PLL).

    As far as the maximum frequency, that is greatly dependent on the quality of your code.  In the case of 'perfect code' the maximum is several hundred megahertz.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • deaxman
    0 deaxman over 12 years ago in reply to e14 Contributor

    What do you mean by "quality".  If there is a lot of code and a lot of resources are used but it is high quality (as in very efficent) does that mean that it is better than something that uses less resources but is less efficent?  Or is this maximum clock speed entirely dependant on the amount of resources used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • deaxman
    0 deaxman over 12 years ago in reply to e14 Contributor

    What do you mean by "quality".  If there is a lot of code and a lot of resources are used but it is high quality (as in very efficent) does that mean that it is better than something that uses less resources but is less efficent?  Or is this maximum clock speed entirely dependant on the amount of resources used?