Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ZynqIntro LAB 5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 824 views
  • Users 0 members are here
Related

ZynqIntro LAB 5

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I started with my new RevD Zedboard. Happy to have the zedboard. I could succefull do the first 4 labs of the ZynqIntro provided in the website. But in the lab 5, i could do up to programming the system.bit, then i was trying to do the launch on hardware then it is giving the error " An internal error occurred during: "Launching LED_Dimmer.elf".
No Target with ID 64 in the System "

Can any help? I am using ISE design suite 14.6

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 12 years ago

    If programming the system.bit works, then that confirms that your JTAG cable, drivers, and software are all OK. Can you confirm that you see the blue DONE LED light up?

     

    However, SDK can't find the ARM when you try to download the ELF. Are you sure you have the MODE jumpers set for Cascaded JTAG?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to bhfletcher

    Hi Bryan, Yes. the blue LED lights up and MODE jumpers are in Cascaded JTAG. What else can be the bug?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I'm also getting that error from time to time in SDK. I fear some configuration is getting messed up accidentally by some unknown action. The only thing that has helped me so far is creating the SDK-project from scratch. But then it happens that shortly after it is broken again. Luckily, I can still use XMD directly to download the bitstream and program:

    XMD% connect arm hw
    XMD% fpga -f /path/to/bitfile.bit
    XMD% source /path/to/hw_platform_spec/ps7_init.tcl
    XMD% ps7_init
    XMD% dow /path/to/program.elf
    XMD% con

    Hope that helps for now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I had the exact same problem. I was able to flash the using XMD. Here are the commands I used in the windows version of the XMD program:

    fpga -f c:tempdesign_1_wrapper.bit
    source c:tempps7_init.tcl
    ps7_init
    cd {c:temp}
    dow HelloWorld.elf