Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ZynqIntro LAB 5
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 825 views
  • Users 0 members are here
Related

ZynqIntro LAB 5

e14 Contributor
e14 Contributor over 12 years ago

Hi,
I started with my new RevD Zedboard. Happy to have the zedboard. I could succefull do the first 4 labs of the ZynqIntro provided in the website. But in the lab 5, i could do up to programming the system.bit, then i was trying to do the launch on hardware then it is giving the error " An internal error occurred during: "Launching LED_Dimmer.elf".
No Target with ID 64 in the System "

Can any help? I am using ISE design suite 14.6

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I'm also getting that error from time to time in SDK. I fear some configuration is getting messed up accidentally by some unknown action. The only thing that has helped me so far is creating the SDK-project from scratch. But then it happens that shortly after it is broken again. Luckily, I can still use XMD directly to download the bitstream and program:

    XMD% connect arm hw
    XMD% fpga -f /path/to/bitfile.bit
    XMD% source /path/to/hw_platform_spec/ps7_init.tcl
    XMD% ps7_init
    XMD% dow /path/to/program.elf
    XMD% con

    Hope that helps for now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    I'm also getting that error from time to time in SDK. I fear some configuration is getting messed up accidentally by some unknown action. The only thing that has helped me so far is creating the SDK-project from scratch. But then it happens that shortly after it is broken again. Luckily, I can still use XMD directly to download the bitstream and program:

    XMD% connect arm hw
    XMD% fpga -f /path/to/bitfile.bit
    XMD% source /path/to/hw_platform_spec/ps7_init.tcl
    XMD% ps7_init
    XMD% dow /path/to/program.elf
    XMD% con

    Hope that helps for now.