Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Problem with Implementing Linux on the Zynq-7000 SoC (lab 4.1)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 373 subscribers
  • Views 1237 views
  • Users 0 members are here
Related

Problem with Implementing Linux on the Zynq-7000 SoC (lab 4.1)

e14 Contributor
e14 Contributor over 13 years ago

Hi,

I've gone through both Speedways, (using version 14.4 of the tools), and had no problems until I reached Lab 4.1.

In this lab, I get no Ethernet connection. I then put the files from the lab-solutions onto the SD card, and saw the same behaviour (I believe this eliminates the tools version as the cause of the problem).

Here's the serial output (using the 'solution' files):
Hi,

I've gone through both Speedways, (using version 14.4 of the tools), and had no problems until I reached Lab 4.1.

In this lab, I get no Ethernet connection. I then put the files from the lab-solutions onto the SD card, and saw the same behaviour (I believe this eliminates the tools version as the cause of the problem).

Here's the serial output (using the 'solution' files):

Linux version 3.3.0-14.2-build1-01491-g42fac65-dirty (training@localhost.localdomain) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #1 SMP PREEMPT Fri Oct 5 12:41:56 PDT 2012

CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZedBoard

bootconsole [earlycon0] enabled

Memory policy: ECC disabled, Data cache writealloc

On node 0 totalpages: 131072

free_area_init_node: node 0, pgdat c045e400, node_mem_map c047a000

  Normal zone: 1152 pages used for memmap

  Normal zone: 0 pages reserved

  Normal zone: 129920 pages, LIFO batch:31

PERCPU: Embedded 7 pages/cpu @c0901000 s5696 r8192 d14784 u32768

pcpu-alloc: s5696 r8192 d14784 u32768 alloc=8*4096

pcpu-alloc: [0] 0 [0] 1

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920

Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x2000000,32M earlyprintk maxcpus=2 debug ip=192.168.1.10

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 512MB = 512MB total

Memory: 481808k/481808k available, 42480k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)

    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc040bdc0   (4112 kB)

      .init : 0xc040c000 - 0xc0430640   ( 146 kB)

      .data : 0xc0432000 - 0xc045fd20   ( 184 kB)

       .bss : 0xc045fd44 - 0xc0479f5c   ( 105 kB)

Preemptible hierarchical RCU implementation.

tVerbose stalled-CPUs detection is disabled.

NR_IRQS:128

xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43

Console: colour dummy device 80x30

Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

smp_twd: clock not found: -2

Calibrating local timer... 333.56MHz.

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

Setting up static identity map for 0x2f30a0 - 0x2f30d4

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

Brought up 2 CPUs

SMP: Total of 2 processors activated (2664.03 BogoMIPS).

devtmpfs: initialized

NET: Registered protocol family 16

L310 cache controller enabled

l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B

registering platform device 'pl330' id 0

registering platform device 'arm-pmu' id 0

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000

bio: create slab <bio-0> at 0

gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops

xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Switching to clocksource xttcpss_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP reno registered

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 32768K

xscugtimer xscugtimer.0: ioremap fe00c200 to e080c200 with size 400

pl330 dev 0 probe success

JFFS2 version 2.2. (NAND) (SUMMARY)  u00C2u00A9 2001-2006 Red Hat, Inc.

msgmni has been set to 1005

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

e00.....[ttyPS0] enabled, bootconsole disabled
console [ttyPS0] enabled, bootconsole disabled

xdevcfg f8007000.devcfg: ioremap f8007000 to e0860000 with size 100
brd: module loaded
loop: module loaded
GEM: BASEADDRESS hw: e000b000 virt: e0862000
XEMACPS mii bus: probed
mdio_bus e000b000: error probing PHY at address 0
eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
Xilinx PS USB Device Controller driver (Apr 01, 2011)
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
Linux video capture interface: v2.00
gspca_main: v2.14.0 registered
uvcvideo: Unable to create debugfs directory
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
WDT OF probe
xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe0866000 with timeout 10 seconds
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: Invalid maximum block size, assuming 512 bytes
mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Registering SWP/SWPB emulation handler
Error xylonfb resources
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
GEM: lp->tx_bd ffdfb000 lp->tx_bd_dma 1d762000 lp->tx_skb dd6f2800
GEM: lp->rx_bd ffdfc000 lp->rx_bd_dma 1d761000 lp->rx_skb dd6f2400
GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
eth0: no PHY found
XEMACPS mii bus mii_probe fail.
IP-Config: Failed to open eth0
IP-Config: No network devices available.
RAMDISK: gzip image found at block 0
mmc0: new high speed SDHC card at address b368
mmcblk0: mmc0:b368 SMI   3.69 GiB
mmcblk0: p1
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 144K
Starting rcS...
++ Mounting filesystem
++ Setting up mdev
++ Starting telnet daemon
++ Starting http daemon
++ Starting ftp daemon
++ Starting dropbear (ssh) daemon
rcS Complete
/ #

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Kevin,

    When I first started to use my Zedboard, the Ethernet port was working (I viewed the webpage).

    With the SD card image you provided, I see no activity. Here's the log:

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2013.03.19 09:52:50 =~=~=~=~=~=~=~=~=~=~=~=


    U-Boot 2011.03-dirty (Jan 14 2013 - 17:28:38)

    DRAM:  512 MiB
    MMC:   SDHCI: 0
    Using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   zynq_gem
    Hit any key to stop autoboot:  3 ... 2 ... 1 ... 0
    Copying Linux from SD to RAM...
    Device: SDHCI
    Manufacturer ID: 12
    OEM: 3456
    Name: SMI  
    Tran Speed: 25000000
    Rd Block Len: 512
    SD version 1.10
    High Capacity: Yes
    Capacity: 3967811584
    Bus Width: 1-bit
    reading zImage

    2408560 bytes read
    reading devicetree.dtb

    7376 bytes read
    reading ramdisk32M.image.gz

    8948903 bytes read
    ## Starting application at 0x00008000 ...
    Uncompressing Linux... done, booting the kernel.
    Booting Linux on physical CPU 0

    Linux version 3.3.0-14.2-build1-01491-g42fac65-dirty (training@localhost.localdomain) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #1 SMP PREEMPT Fri Oct 5 12:41:56 PDT 2012

    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

    Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZedBoard

    bootconsole [earlycon0] enabled

    Memory policy: ECC disabled, Data cache writealloc

    On node 0 totalpages: 131072

    free_area_init_node: node 0, pgdat c045e400, node_mem_map c047a000

      Normal zone: 1152 pages used for memmap

      Normal zone: 0 pages reserved

      Normal zone: 129920 pages, LIFO batch:31

    PERCPU: Embedded 7 pages/cpu @c0901000 s5696 r8192 d14784 u32768

    pcpu-alloc: s5696 r8192 d14784 u32768 alloc=8*4096

    pcpu-alloc: [0] 0 [0] 1

    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920

    Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x2000000,32M earlyprintk maxcpus=2 debug ip=192.168.1.10

    PID hash table entries: 2048 (order: 1, 8192 bytes)

    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

    Memory: 512MB = 512MB total

    Memory: 481808k/481808k available, 42480k reserved, 0K highmem

    Virtual kernel memory layout:

        vector  : 0xffff0000 - 0xffff1000   (   4 kB)

        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

        vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)

        lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

        modules : 0xbf000000 - 0xbfe00000   (  14 MB)

          .text : 0xc0008000 - 0xc040bdc0   (4112 kB)

          .init : 0xc040c000 - 0xc0430640   ( 146 kB)

          .data : 0xc0432000 - 0xc045fd20   ( 184 kB)

           .bss : 0xc045fd44 - 0xc0479f5c   ( 105 kB)

    Preemptible hierarchical RCU implementation.

    tVerbose stalled-CPUs detection is disabled.

    NR_IRQS:128

    xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43

    Console: colour dummy device 80x30

    Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)

    pid_max: default: 32768 minimum: 301

    Mount-cache hash table entries: 512

    CPU: Testing write buffer coherency: ok

    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

    smp_twd: clock not found: -2

    Calibrating local timer... 333.56MHz.

    hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

    Setting up static identity map for 0x2f30a0 - 0x2f30d4

    CPU1: Booted secondary processor

    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

    Brought up 2 CPUs

    SMP: Total of 2 processors activated (2664.03 BogoMIPS).

    devtmpfs: initialized

    NET: Registered protocol family 16

    L310 cache controller enabled

    l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B

    registering platform device 'pl330' id 0

    registering platform device 'arm-pmu' id 0

    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

    hw-breakpoint: maximum watchpoint size is 4 bytes.

    xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000

    bio: create slab <bio-0> at 0

    gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops

    xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000

    SCSI subsystem initialized

    usbcore: registered new interface driver usbfs

    usbcore: registered new interface driver hub

    usbcore: registered new device driver usb

    Switching to clocksource xttcpss_timer1

    NET: Registered protocol family 2

    IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

    TCP established hash table entries: 16384 (order: 5, 131072 bytes)

    TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

    TCP: Hash tables configured (established 16384 bind 16384)

    TCP reno registered

    UDP hash table entries: 256 (order: 1, 8192 bytes)

    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

    NET: Registered protocol family 1

    RPC: Registered named UNIX socket transport module.

    RPC: Registered udp transport module.

    RPC: Registered tcp transport module.

    RPC: Registered tcp NFSv4.1 backchannel transport module.

    Trying to unpack rootfs image as initramfs...

    rootfs image is not initramfs (no cpio magic); looks like an initrd

    Freeing initrd memory: 32768K

    xscugtimer xscugtimer.0: ioremap fe00c200 to e080c200 with size 400

    pl330 dev 0 probe success

    JFFS2 version 2.2. (NAND) (SUMMARY)  -u00A9 2001-2006 Red Hat, Inc.

    msgmni has been set to 1005

    io scheduler noop registered

    io scheduler deadline registered

    io scheduler cfq registered (default)

    e00------[ttyPS0] enabled, bootconsole disabled
    console [ttyPS0] enabled, bootconsole disabled

    xdevcfg f8007000.devcfg: ioremap f8007000 to e0860000 with size 100
    brd: module loaded
    loop: module loaded
    GEM: BASEADDRESS hw: e000b000 virt: e0862000
    XEMACPS mii bus: probed
    mdio_bus e000b000: error probing PHY at address 0
    eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
    xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
    xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
    xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    Xilinx PS USB Device Controller driver (Apr 01, 2011)
    mousedev: PS/2 mouse device common for all mice
    i2c /dev entries driver
    Linux video capture interface: v2.00
    gspca_main: v2.14.0 registered
    uvcvideo: Unable to create debugfs directory
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (1.1.1)
    WDT OF probe
    xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe0866000 with timeout 10 seconds
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    mmc0: Invalid maximum block size, assuming 512 bytes
    mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    TCP cubic registered
    NET: Registered protocol family 17
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    Registering SWP/SWPB emulation handler
    Error xylonfb resources
    drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    GEM: lp->tx_bd ffdfb000 lp->tx_bd_dma 1d762000 lp->tx_skb dd6f2800
    GEM: lp->rx_bd ffdfc000 lp->rx_bd_dma 1d761000 lp->rx_skb dd6f2400
    GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
    eth0: no PHY found
    XEMACPS mii bus mii_probe fail.
    IP-Config: Failed to open eth0
    IP-Config: No network devices available.
    RAMDISK: gzip image found at block 0
    mmc0: new high speed SDHC card at address b368
    mmcblk0: mmc0:b368 SMI   3.69 GiB
    mmcblk0: p1
    VFS: Mounted root (ext2 filesystem) on device 1:0.
    devtmpfs: mounted
    Freeing init memory: 144K
    Starting rcS...
    ++ Mounting filesystem
    ++ Setting up mdev
    ++ Starting telnet daemon
    ++ Starting http daemon
    ++ Starting ftp daemon
    ++ Starting dropbear (ssh) daemon
    rcS Complete
    / #


    Looks like the Ethernet device is dead.

    So I suppose I need a replacement board. Would it be possible to contact David Gregg in the UK to approve this?

    Thanks,

    - Brendan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Kevin,

    When I first started to use my Zedboard, the Ethernet port was working (I viewed the webpage).

    With the SD card image you provided, I see no activity. Here's the log:

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2013.03.19 09:52:50 =~=~=~=~=~=~=~=~=~=~=~=


    U-Boot 2011.03-dirty (Jan 14 2013 - 17:28:38)

    DRAM:  512 MiB
    MMC:   SDHCI: 0
    Using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   zynq_gem
    Hit any key to stop autoboot:  3 ... 2 ... 1 ... 0
    Copying Linux from SD to RAM...
    Device: SDHCI
    Manufacturer ID: 12
    OEM: 3456
    Name: SMI  
    Tran Speed: 25000000
    Rd Block Len: 512
    SD version 1.10
    High Capacity: Yes
    Capacity: 3967811584
    Bus Width: 1-bit
    reading zImage

    2408560 bytes read
    reading devicetree.dtb

    7376 bytes read
    reading ramdisk32M.image.gz

    8948903 bytes read
    ## Starting application at 0x00008000 ...
    Uncompressing Linux... done, booting the kernel.
    Booting Linux on physical CPU 0

    Linux version 3.3.0-14.2-build1-01491-g42fac65-dirty (training@localhost.localdomain) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #1 SMP PREEMPT Fri Oct 5 12:41:56 PDT 2012

    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

    Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZedBoard

    bootconsole [earlycon0] enabled

    Memory policy: ECC disabled, Data cache writealloc

    On node 0 totalpages: 131072

    free_area_init_node: node 0, pgdat c045e400, node_mem_map c047a000

      Normal zone: 1152 pages used for memmap

      Normal zone: 0 pages reserved

      Normal zone: 129920 pages, LIFO batch:31

    PERCPU: Embedded 7 pages/cpu @c0901000 s5696 r8192 d14784 u32768

    pcpu-alloc: s5696 r8192 d14784 u32768 alloc=8*4096

    pcpu-alloc: [0] 0 [0] 1

    Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920

    Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x2000000,32M earlyprintk maxcpus=2 debug ip=192.168.1.10

    PID hash table entries: 2048 (order: 1, 8192 bytes)

    Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

    Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

    Memory: 512MB = 512MB total

    Memory: 481808k/481808k available, 42480k reserved, 0K highmem

    Virtual kernel memory layout:

        vector  : 0xffff0000 - 0xffff1000   (   4 kB)

        fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

        vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)

        lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

        modules : 0xbf000000 - 0xbfe00000   (  14 MB)

          .text : 0xc0008000 - 0xc040bdc0   (4112 kB)

          .init : 0xc040c000 - 0xc0430640   ( 146 kB)

          .data : 0xc0432000 - 0xc045fd20   ( 184 kB)

           .bss : 0xc045fd44 - 0xc0479f5c   ( 105 kB)

    Preemptible hierarchical RCU implementation.

    tVerbose stalled-CPUs detection is disabled.

    NR_IRQS:128

    xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43

    Console: colour dummy device 80x30

    Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)

    pid_max: default: 32768 minimum: 301

    Mount-cache hash table entries: 512

    CPU: Testing write buffer coherency: ok

    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

    smp_twd: clock not found: -2

    Calibrating local timer... 333.56MHz.

    hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

    Setting up static identity map for 0x2f30a0 - 0x2f30d4

    CPU1: Booted secondary processor

    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

    Brought up 2 CPUs

    SMP: Total of 2 processors activated (2664.03 BogoMIPS).

    devtmpfs: initialized

    NET: Registered protocol family 16

    L310 cache controller enabled

    l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B

    registering platform device 'pl330' id 0

    registering platform device 'arm-pmu' id 0

    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

    hw-breakpoint: maximum watchpoint size is 4 bytes.

    xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000

    bio: create slab <bio-0> at 0

    gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops

    xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000

    SCSI subsystem initialized

    usbcore: registered new interface driver usbfs

    usbcore: registered new interface driver hub

    usbcore: registered new device driver usb

    Switching to clocksource xttcpss_timer1

    NET: Registered protocol family 2

    IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

    TCP established hash table entries: 16384 (order: 5, 131072 bytes)

    TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

    TCP: Hash tables configured (established 16384 bind 16384)

    TCP reno registered

    UDP hash table entries: 256 (order: 1, 8192 bytes)

    UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

    NET: Registered protocol family 1

    RPC: Registered named UNIX socket transport module.

    RPC: Registered udp transport module.

    RPC: Registered tcp transport module.

    RPC: Registered tcp NFSv4.1 backchannel transport module.

    Trying to unpack rootfs image as initramfs...

    rootfs image is not initramfs (no cpio magic); looks like an initrd

    Freeing initrd memory: 32768K

    xscugtimer xscugtimer.0: ioremap fe00c200 to e080c200 with size 400

    pl330 dev 0 probe success

    JFFS2 version 2.2. (NAND) (SUMMARY)  -u00A9 2001-2006 Red Hat, Inc.

    msgmni has been set to 1005

    io scheduler noop registered

    io scheduler deadline registered

    io scheduler cfq registered (default)

    e00------[ttyPS0] enabled, bootconsole disabled
    console [ttyPS0] enabled, bootconsole disabled

    xdevcfg f8007000.devcfg: ioremap f8007000 to e0860000 with size 100
    brd: module loaded
    loop: module loaded
    GEM: BASEADDRESS hw: e000b000 virt: e0862000
    XEMACPS mii bus: probed
    mdio_bus e000b000: error probing PHY at address 0
    eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
    xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
    xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
    xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    Xilinx PS USB Device Controller driver (Apr 01, 2011)
    mousedev: PS/2 mouse device common for all mice
    i2c /dev entries driver
    Linux video capture interface: v2.00
    gspca_main: v2.14.0 registered
    uvcvideo: Unable to create debugfs directory
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (1.1.1)
    WDT OF probe
    xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe0866000 with timeout 10 seconds
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    mmc0: Invalid maximum block size, assuming 512 bytes
    mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    TCP cubic registered
    NET: Registered protocol family 17
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    Registering SWP/SWPB emulation handler
    Error xylonfb resources
    drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    GEM: lp->tx_bd ffdfb000 lp->tx_bd_dma 1d762000 lp->tx_skb dd6f2800
    GEM: lp->rx_bd ffdfc000 lp->rx_bd_dma 1d761000 lp->rx_skb dd6f2400
    GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
    eth0: no PHY found
    XEMACPS mii bus mii_probe fail.
    IP-Config: Failed to open eth0
    IP-Config: No network devices available.
    RAMDISK: gzip image found at block 0
    mmc0: new high speed SDHC card at address b368
    mmcblk0: mmc0:b368 SMI   3.69 GiB
    mmcblk0: p1
    VFS: Mounted root (ext2 filesystem) on device 1:0.
    devtmpfs: mounted
    Freeing init memory: 144K
    Starting rcS...
    ++ Mounting filesystem
    ++ Setting up mdev
    ++ Starting telnet daemon
    ++ Starting http daemon
    ++ Starting ftp daemon
    ++ Starting dropbear (ssh) daemon
    rcS Complete
    / #


    Looks like the Ethernet device is dead.

    So I suppose I need a replacement board. Would it be possible to contact David Gregg in the UK to approve this?

    Thanks,

    - Brendan