Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Problem with Implementing Linux on the Zynq-7000 SoC (lab 4.1)
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 373 subscribers
  • Views 1237 views
  • Users 0 members are here
Related

Problem with Implementing Linux on the Zynq-7000 SoC (lab 4.1)

e14 Contributor
e14 Contributor over 13 years ago

Hi,

I've gone through both Speedways, (using version 14.4 of the tools), and had no problems until I reached Lab 4.1.

In this lab, I get no Ethernet connection. I then put the files from the lab-solutions onto the SD card, and saw the same behaviour (I believe this eliminates the tools version as the cause of the problem).

Here's the serial output (using the 'solution' files):
Hi,

I've gone through both Speedways, (using version 14.4 of the tools), and had no problems until I reached Lab 4.1.

In this lab, I get no Ethernet connection. I then put the files from the lab-solutions onto the SD card, and saw the same behaviour (I believe this eliminates the tools version as the cause of the problem).

Here's the serial output (using the 'solution' files):

Linux version 3.3.0-14.2-build1-01491-g42fac65-dirty (training@localhost.localdomain) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #1 SMP PREEMPT Fri Oct 5 12:41:56 PDT 2012

CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZedBoard

bootconsole [earlycon0] enabled

Memory policy: ECC disabled, Data cache writealloc

On node 0 totalpages: 131072

free_area_init_node: node 0, pgdat c045e400, node_mem_map c047a000

  Normal zone: 1152 pages used for memmap

  Normal zone: 0 pages reserved

  Normal zone: 129920 pages, LIFO batch:31

PERCPU: Embedded 7 pages/cpu @c0901000 s5696 r8192 d14784 u32768

pcpu-alloc: s5696 r8192 d14784 u32768 alloc=8*4096

pcpu-alloc: [0] 0 [0] 1

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 129920

Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x2000000,32M earlyprintk maxcpus=2 debug ip=192.168.1.10

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 512MB = 512MB total

Memory: 481808k/481808k available, 42480k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    vmalloc : 0xe0800000 - 0xff000000   ( 488 MB)

    lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    modules : 0xbf000000 - 0xbfe00000   (  14 MB)

      .text : 0xc0008000 - 0xc040bdc0   (4112 kB)

      .init : 0xc040c000 - 0xc0430640   ( 146 kB)

      .data : 0xc0432000 - 0xc045fd20   ( 184 kB)

       .bss : 0xc045fd44 - 0xc0479f5c   ( 105 kB)

Preemptible hierarchical RCU implementation.

tVerbose stalled-CPUs detection is disabled.

NR_IRQS:128

xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43

Console: colour dummy device 80x30

Calibrating delay loop... 1332.01 BogoMIPS (lpj=6660096)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

smp_twd: clock not found: -2

Calibrating local timer... 333.56MHz.

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

Setting up static identity map for 0x2f30a0 - 0x2f30d4

CPU1: Booted secondary processor

CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

Brought up 2 CPUs

SMP: Total of 2 processors activated (2664.03 BogoMIPS).

devtmpfs: initialized

NET: Registered protocol family 16

L310 cache controller enabled

l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72360000, Cache size: 524288 B

registering platform device 'pl330' id 0

registering platform device 'arm-pmu' id 0

hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 4 bytes.

xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000

bio: create slab <bio-0> at 0

gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops

xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Switching to clocksource xttcpss_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

TCP established hash table entries: 16384 (order: 5, 131072 bytes)

TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

TCP: Hash tables configured (established 16384 bind 16384)

TCP reno registered

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

Trying to unpack rootfs image as initramfs...

rootfs image is not initramfs (no cpio magic); looks like an initrd

Freeing initrd memory: 32768K

xscugtimer xscugtimer.0: ioremap fe00c200 to e080c200 with size 400

pl330 dev 0 probe success

JFFS2 version 2.2. (NAND) (SUMMARY)  u00C2u00A9 2001-2006 Red Hat, Inc.

msgmni has been set to 1005

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

e00.....[ttyPS0] enabled, bootconsole disabled
console [ttyPS0] enabled, bootconsole disabled

xdevcfg f8007000.devcfg: ioremap f8007000 to e0860000 with size 100
brd: module loaded
loop: module loaded
GEM: BASEADDRESS hw: e000b000 virt: e0862000
XEMACPS mii bus: probed
mdio_bus e000b000: error probing PHY at address 0
eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
Xilinx PS USB Device Controller driver (Apr 01, 2011)
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
Linux video capture interface: v2.00
gspca_main: v2.14.0 registered
uvcvideo: Unable to create debugfs directory
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
WDT OF probe
xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe0866000 with timeout 10 seconds
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: Invalid maximum block size, assuming 512 bytes
mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
TCP cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Registering SWP/SWPB emulation handler
Error xylonfb resources
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
GEM: lp->tx_bd ffdfb000 lp->tx_bd_dma 1d762000 lp->tx_skb dd6f2800
GEM: lp->rx_bd ffdfc000 lp->rx_bd_dma 1d761000 lp->rx_skb dd6f2400
GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
eth0: no PHY found
XEMACPS mii bus mii_probe fail.
IP-Config: Failed to open eth0
IP-Config: No network devices available.
RAMDISK: gzip image found at block 0
mmc0: new high speed SDHC card at address b368
mmcblk0: mmc0:b368 SMI   3.69 GiB
mmcblk0: p1
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing init memory: 144K
Starting rcS...
++ Mounting filesystem
++ Setting up mdev
++ Starting telnet daemon
++ Starting http daemon
++ Starting ftp daemon
++ Starting dropbear (ssh) daemon
rcS Complete
/ #

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Wait, apologies - I sent you an old log file. Here's the log file associated with the OOB SD image:

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2013.03.21 10:43:18 =~=~=~=~=~=~=~=~=~=~=~=


    U-Boot 2012.04.01-00297-gc319bf9-dirty (Sep 13 2012 - 09:30:49)

    DRAM:  512 MiB
    WARNING: Caches not enabled
    MMC:   SDHCI: 0
    Using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   zynq_gem
    Hit any key to stop autoboot:  3  2  1  0
    Copying Linux from SD to RAM...
    Device: SDHCI
    Manufacturer ID: 12
    OEM: 3456
    Name: SMI  
    Tran Speed: 25000000
    Rd Block Len: 512
    SD version 1.0
    High Capacity: Yes
    Capacity: 3.7 GiB
    Bus Width: 1-bit
    reading zImage

    2479640 bytes read
    reading devicetree_ramdisk.dtb

    5817 bytes read
    reading ramdisk8M.image.gz

    3694108 bytes read
    ## Starting application at 0x00008000 ...
    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Booting Linux on physical CPU 0

    [    0.000000] Linux version 3.3.0-digilent-12.07-zed-beta (tinghui.wang@DIGILENT_LINUX) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #2 SMP PREEMPT Thu Jul 12 21:01:42 PDT 2012

    [    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

    [    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED

    [    0.000000] bootconsole [earlycon0] enabled

    [    0.000000] Memory policy: ECC disabled, Data cache writealloc

    [    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space

    [    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space

    [    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space

    [    0.000000] PERCPU: Embedded 7 pages/cpu @c1489000 s5696 r8192 d14784 u32768

    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824

    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0

    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)

    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

    [    0.000000] Memory: 240MB 256MB = 496MB total

    [    0.000000] Memory: 489856k/489856k available, 34432k reserved, 0K highmem

    [    0.000000] Virtual kernel memory layout:

    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    [    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)

    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

    [    0.000000]       .text : 0xc0008000 - 0xc042f040   (4253 kB)

    [    0.000000]       .init : 0xc0430000 - 0xc0456640   ( 154 kB)

    [    0.000000]       .data : 0xc0458000 - 0xc0485dc0   ( 184 kB)

    [    0.000000]        .bss : 0xc0485de4 - 0xc049d734   (  95 kB)

    [    0.000000] Preemptible hierarchical RCU implementation.

    [    0.000000] Verbose stalled-CPUs detection is disabled.

    [    0.000000] NR_IRQS:128

    [    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43

    [    0.000000] Console: colour dummy device 80x30

    [    0.000000] Calibrating delay loop... 1594.16 BogoMIPS (lpj=7970816)

    [    0.090000] pid_max: default: 32768 minimum: 301

    [    0.090000] Mount-cache hash table entries: 512

    [    0.090000] CPU: Testing write buffer coherency: ok

    [    0.090000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

    [    0.100000] smp_twd: clock not found: -2

    [    0.100000] Calibrating local timer... 399.37MHz.

    [    0.170000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

    [    0.170000] Setting up static identity map for 0x2f8d48 - 0x2f8d7c

    [    0.270000] CPU1: Booted secondary processor

    [    0.310000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

    [    0.310000] Brought up 2 CPUs

    [    0.310000] SMP: Total of 2 processors activated (3188.32 BogoMIPS).

    [    0.320000] devtmpfs: initialized

    [    0.320000] ------------[ cut here ]------------

    [    0.320000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()

    [    0.330000] Modules linked in:

    [    0.330000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)

    [    0.340000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)

    [    0.350000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)

    [    0.360000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)

    [    0.360000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)

    [    0.370000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)

    [    0.380000] ---[ end trace 1b75b31a2719ed1c ]---

    [    0.380000] ------------[ cut here ]------------

    [    0.390000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()

    [    0.390000] Modules linked in:

    [    0.390000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)

    [    0.400000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)

    [    0.410000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)

    [    0.420000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)

    [    0.430000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)

    [    0.430000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)

    [    0.440000] ---[ end trace 1b75b31a2719ed1d ]---

    [    0.440000] NET: Registered protocol family 16

    [    0.460000] L310 cache controller enabled

    [    0.460000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72060000, Cache size: 524288 B

    [    0.460000] registering platform device 'pl330' id 0

    [    0.470000] registering platform device 'arm-pmu' id 0

    [    0.470000]

    [    0.470000] ###############################################

    [    0.480000] #                                             #

    [    0.480000] #                Board ZED Init               #

    [    0.480000] #                                             #

    [    0.490000] ###############################################

    [    0.490000]

    [    0.500000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

    [    0.500000] hw-breakpoint: maximum watchpoint size is 4 bytes.

    [    0.530000] xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000

    [    0.540000] bio: create slab <bio-0> at 0

    [    0.540000] gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops

    [    0.540000] xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000

    [    0.550000] SCSI subsystem initialized

    [    0.550000] usbcore: registered new interface driver usbfs

    [    0.560000] usbcore: registered new interface driver hub

    [    0.560000] usbcore: registered new device driver usb

    [    0.570000] Advanced Linux Sound Architecture Driver Version 1.0.24.

    [    0.570000] Switching to clocksource xttcpss_timer1

    [    0.590000] NET: Registered protocol family 2

    [    0.590000] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

    [    0.590000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)

    [    0.600000] TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

    [    0.600000] TCP: Hash tables configured (established 16384 bind 16384)

    [    0.610000] TCP reno registered

    [    0.610000] UDP hash table entries: 256 (order: 1, 8192 bytes)

    [    0.620000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

    [    0.620000] NET: Registered protocol family 1

    [    0.630000] Trying to unpack rootfs image as initramfs...

    [    0.630000] rootfs image is not initramfs (no cpio magic); looks like an initrd

    [    0.670000] Freeing initrd memory: 8192K

    [    0.670000] xscugtimer xscugtimer.0: ioremap fe00c200 to e0810200 with size 400

    [    0.670000] pl330 dev 0 probe success

    [    0.680000] msgmni has been set to 972

    [    0.680000] io scheduler noop registered

    [    0.680000] io scheduler deadline registered

    [    0.680000] io scheduler cfq registered (default)

    [    0.690000] e00   0.690000] console [ttyPS0] enabled, bootconsole disabled
    [    0.690000] console [ttyPS0] enabled, bootconsole disabled

    [    0.700000] xdevcfg f8007000.devcfg: ioremap f8007000 to e0814000 with size 1000
    [    0.710000] [drm] Initialized drm 1.1.0 20060810
    [    0.720000] brd: module loaded
    [    0.730000] loop: module loaded
    [    0.730000] xqspips e000d000.qspi: at 0xE000D000 mapped to 0xE0816000, irq=51
    [    0.740000] GEM: BASEADDRESS hw: e000b000 virt: e0818000
    [    0.740000] XEMACPS mii bus: probed
    [    0.750000] mdio_bus c0197b60: error probing PHY at address 0
    [    0.750000] eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
    [    0.760000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    0.760000] usb_hcd_xusbps_probe: No OTG assigned!
    [    0.770000] usb_hcd_xusbps_probe: OTG now assigned!
    [    0.770000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
    [    0.780000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
    [    0.810000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
    [    0.830000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
    [    0.830000] hub 1-0:1.0: USB hub found
    [    0.830000] hub 1-0:1.0: 1 port detected
    [    0.840000] Initializing USB Mass Storage driver...
    [    0.840000] usbcore: registered new interface driver usb-storage
    [    0.850000] USB Mass Storage support registered.
    [    0.850000] Xilinx PS USB Device Controller driver (Apr 01, 2011)
    [    0.860000] mousedev: PS/2 mouse device common for all mice
    [    0.860000] Linux video capture interface: v2.00
    [    0.870000] gspca_main: v2.14.0 registered
    [    0.870000] usbcore: registered new interface driver uvcvideo
    [    0.870000] USB Video Class driver (1.1.1)
    [    0.880000] WDT OF probe
    [    0.880000] xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe081c000 with timeout 10 seconds
    [    0.890000] sdhci: Secure Digital Host Controller Interface driver
    [    0.890000] sdhci: Copyright(c) Pierre Ossman
    [    0.900000] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.900000] mmc0: Invalid maximum block size, assuming 512 bytes
    [    0.910000] mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
    [    0.920000] usbcore: registered new interface driver usbhid
    [    0.920000] usbhid: USB HID core driver
    [    0.930000] edid status: 1
    [    0.930000] adv7511 0-0039: Failed to add route DAI IN->TMDS
    [    0.950000] asoc: adv7511 <-> 75c00000.axi-spdif-tx mapping ok
    [    0.950000] axi-spdif 75c00000.axi-spdif-tx: Failed to set DAI format: -22
    [    0.960000] ALSA device list:
    [    0.960000]   #0: HDMI monitor
    [    0.970000] TCP cubic registered
    [    0.970000] NET: Registered protocol family 17
    [    0.970000] edid ret: 4
    [    0.980000] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    [    0.980000] Registering SWP/SWPB emulation handler
    [    0.990000] registered taskstats version 1
    [    0.990000] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    [    0.990000] i2c ret: 2
    [    1.000000] mmc0: new high speed SDHC card at address b368
    [    1.000000] mmcblk0: mmc0:b368 SMI   3.69 GiB
    [    1.010000]  mmcblk0: p1
    [    1.010000] RAMDISK: gzip image found at block 0
    [    1.010000] i2c ret: 2
    [    1.020000] i2c ret: 2
    [    1.030000] i2c ret: 2
    [    1.030000] new mode: 1920x1080 2080x1111 138500
    [    1.030000] new mode: 1680x1050 2240x1089 146250
    [    1.040000] new mode: 1280x720 1650x750 74250
    [    1.040000] new mode: 1920x1080 2200x1125 74250
    [    1.050000] new mode: 720x480 858x525 27000
    [    1.050000] new mode: 720x480 858x525 27000
    [    1.050000] new mode: 1920x1080 2200x1125 148500
    [    1.060000] new mode: 1280x1024 1688x1066 108000
    [    1.060000] new mode: 1280x1024 1688x1066 135000
    [    1.060000] new mode: 1152x864 1520x895 81579
    [    1.070000] new mode: 1280x960 1728x1002 129936
    [    1.070000] new mode: 1152x864 1600x900 108000
    [    1.080000] new mode: 800x600 1056x628 40000
    [    1.080000] new mode: 640x480 840x500 31500
    [    1.080000] new mode: 640x480 800x525 25200
    [    1.090000] new mode: 720x400 900x449 28320
    [    1.090000] new mode: 1280x1024 1688x1066 135000
    [    1.090000] new mode: 1024x768 1312x800 78800
    [    1.100000] new mode: 1024x768 1328x806 75000
    [    1.100000] new mode: 1024x768 1344x806 65000
    [    1.100000] new mode: 832x624 1152x667 57284
    [    1.110000] new mode: 800x600 1056x625 49500
    [    1.110000] new mode: 1280x720 1650x750 74250
    [    1.110000] new mode: 1920x1080 2200x1125 74250
    [    1.120000] new mode: 720x480 858x525 27000
    [    1.120000] new mode: 720x480 858x525 27000
    [    1.120000] new mode: 1920x1080 2750x1125 74250
    [    1.130000] new mode: 1920x1080 2200x1125 74250
    [    1.130000] new mode: 1920x1080 2200x1125 148500
    [    1.140000] new mode: 720x576 864x625 27000
    [    1.140000] new mode: 1280x720 1980x750 74250
    [    1.140000] new mode: 720x576 864x625 27000
    [    1.150000] new mode: 1920x1080 2640x1125 74250
    [    1.150000] new mode: 1920x1080 2640x1125 148500
    [    1.150000] new mode: 1440x480 1716x525 27000
    [    1.160000] new mode: 1440x576 1728x625 27000
    [    1.180000] drivers/gpu/drm/analog/analog_drm_fbdev.c:analog_drm_fbdev_probe[241]
    [    1.180000] setting clock to: 138500
    [    1.180000] raw_edid: d816bac0 7
    [    1.180000] Using YCbCr output
    [    1.220000] Console: switching to colour frame buffer device 240x67
    [    1.260000] fb0:  frame buffer device
    [    1.260000] drm: registered panic notifier
    [    1.270000] [drm] Initialized analog_drm 1.0.0 20110530 on minor 0
    [    1.280000] EXT4-fs (ram0): warning: mounting unchecked fs, running e2fsck is recommended
    [    1.280000] EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
    [    1.290000] VFS: Mounted root (ext4 filesystem) on device 1:0.
    [    1.300000] Freeing init memory: 152K
    Starting rcS...
    ++ Mounting filesystem
    ++ Setting up mdev
    ++ Configure static IP 192.168.1.10
    [    1.480000] GEM: lp->tx_bd ffdfa000 lp->tx_bd_dma 18bd6000 lp->tx_skb d8ac39c0
    [    1.490000] GEM: lp->rx_bd ffdfb000 lp->rx_bd_dma 18bd5000 lp->rx_skb d8ac3ac0
    [    1.490000] GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
    [    1.500000] eth0: no PHY found
    [    1.500000] XEMACPS mii bus mii_probe fail.
    ifconfig: SIOCSIFFLAGS: No such device or address
    ++ Starting telnet daemon
    ++ Starting http daemon
    ++ Starting ftp daemon
    ++ Starting dropbear (ssh) daemon
    ++ Starting OLED Display
    [    1.550000] pmodoled-gpio-spi [zed_oled] SPI Probing
    ++ Exporting LEDs & SWs
    rcS Complete
    zynq>


    Cheers,

    - Bren

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Wait, apologies - I sent you an old log file. Here's the log file associated with the OOB SD image:

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2013.03.21 10:43:18 =~=~=~=~=~=~=~=~=~=~=~=


    U-Boot 2012.04.01-00297-gc319bf9-dirty (Sep 13 2012 - 09:30:49)

    DRAM:  512 MiB
    WARNING: Caches not enabled
    MMC:   SDHCI: 0
    Using default environment

    In:    serial
    Out:   serial
    Err:   serial
    Net:   zynq_gem
    Hit any key to stop autoboot:  3  2  1  0
    Copying Linux from SD to RAM...
    Device: SDHCI
    Manufacturer ID: 12
    OEM: 3456
    Name: SMI  
    Tran Speed: 25000000
    Rd Block Len: 512
    SD version 1.0
    High Capacity: Yes
    Capacity: 3.7 GiB
    Bus Width: 1-bit
    reading zImage

    2479640 bytes read
    reading devicetree_ramdisk.dtb

    5817 bytes read
    reading ramdisk8M.image.gz

    3694108 bytes read
    ## Starting application at 0x00008000 ...
    Uncompressing Linux... done, booting the kernel.
    [    0.000000] Booting Linux on physical CPU 0

    [    0.000000] Linux version 3.3.0-digilent-12.07-zed-beta (tinghui.wang@DIGILENT_LINUX) (gcc version 4.6.1 (Sourcery CodeBench Lite 2011.09-50) ) #2 SMP PREEMPT Thu Jul 12 21:01:42 PDT 2012

    [    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d

    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

    [    0.000000] Machine: Xilinx Zynq Platform, model: Xilinx Zynq ZED

    [    0.000000] bootconsole [earlycon0] enabled

    [    0.000000] Memory policy: ECC disabled, Data cache writealloc

    [    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space

    [    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space

    [    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space

    [    0.000000] PERCPU: Embedded 7 pages/cpu @c1489000 s5696 r8192 d14784 u32768

    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 125824

    [    0.000000] Kernel command line: console=ttyPS0,115200 root=/dev/ram rw initrd=0x800000,8M earlyprintk rootfstype=ext4 rootwait devtmpfs.mount=0

    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)

    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

    [    0.000000] Memory: 240MB 256MB = 496MB total

    [    0.000000] Memory: 489856k/489856k available, 34432k reserved, 0K highmem

    [    0.000000] Virtual kernel memory layout:

    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    [    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)

    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)

    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

    [    0.000000]       .text : 0xc0008000 - 0xc042f040   (4253 kB)

    [    0.000000]       .init : 0xc0430000 - 0xc0456640   ( 154 kB)

    [    0.000000]       .data : 0xc0458000 - 0xc0485dc0   ( 184 kB)

    [    0.000000]        .bss : 0xc0485de4 - 0xc049d734   (  95 kB)

    [    0.000000] Preemptible hierarchical RCU implementation.

    [    0.000000] Verbose stalled-CPUs detection is disabled.

    [    0.000000] NR_IRQS:128

    [    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43

    [    0.000000] Console: colour dummy device 80x30

    [    0.000000] Calibrating delay loop... 1594.16 BogoMIPS (lpj=7970816)

    [    0.090000] pid_max: default: 32768 minimum: 301

    [    0.090000] Mount-cache hash table entries: 512

    [    0.090000] CPU: Testing write buffer coherency: ok

    [    0.090000] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

    [    0.100000] smp_twd: clock not found: -2

    [    0.100000] Calibrating local timer... 399.37MHz.

    [    0.170000] hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

    [    0.170000] Setting up static identity map for 0x2f8d48 - 0x2f8d7c

    [    0.270000] CPU1: Booted secondary processor

    [    0.310000] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001

    [    0.310000] Brought up 2 CPUs

    [    0.310000] SMP: Total of 2 processors activated (3188.32 BogoMIPS).

    [    0.320000] devtmpfs: initialized

    [    0.320000] ------------[ cut here ]------------

    [    0.320000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()

    [    0.330000] Modules linked in:

    [    0.330000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)

    [    0.340000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)

    [    0.350000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)

    [    0.360000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)

    [    0.360000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)

    [    0.370000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)

    [    0.380000] ---[ end trace 1b75b31a2719ed1c ]---

    [    0.380000] ------------[ cut here ]------------

    [    0.390000] WARNING: at arch/arm/mm/dma-mapping.c:198 consistent_init+0x70/0x104()

    [    0.390000] Modules linked in:

    [    0.390000] [<c0012920>] (unwind_backtrace+0x0/0xe0) from [<c001e924>] (warn_slowpath_common+0x4c/0x64)

    [    0.400000] [<c001e924>] (warn_slowpath_common+0x4c/0x64) from [<c001e954>] (warn_slowpath_null+0x18/0x1c)

    [    0.410000] [<c001e954>] (warn_slowpath_null+0x18/0x1c) from [<c04345a8>] (consistent_init+0x70/0x104)

    [    0.420000] [<c04345a8>] (consistent_init+0x70/0x104) from [<c000858c>] (do_one_initcall+0x90/0x160)

    [    0.430000] [<c000858c>] (do_one_initcall+0x90/0x160) from [<c043085c>] (kernel_init+0x84/0x128)

    [    0.430000] [<c043085c>] (kernel_init+0x84/0x128) from [<c000dfcc>] (kernel_thread_exit+0x0/0x8)

    [    0.440000] ---[ end trace 1b75b31a2719ed1d ]---

    [    0.440000] NET: Registered protocol family 16

    [    0.460000] L310 cache controller enabled

    [    0.460000] l2x0: 8 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x72060000, Cache size: 524288 B

    [    0.460000] registering platform device 'pl330' id 0

    [    0.470000] registering platform device 'arm-pmu' id 0

    [    0.470000]

    [    0.470000] ###############################################

    [    0.480000] #                                             #

    [    0.480000] #                Board ZED Init               #

    [    0.480000] #                                             #

    [    0.490000] ###############################################

    [    0.490000]

    [    0.500000] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.

    [    0.500000] hw-breakpoint: maximum watchpoint size is 4 bytes.

    [    0.530000] xslcr xslcr.0: at 0xF8000000 mapped to 0xE0808000

    [    0.540000] bio: create slab <bio-0> at 0

    [    0.540000] gpiochip_add: registered GPIOs 0 to 245 on device: xgpiops

    [    0.540000] xgpiops e000a000.gpio: gpio at 0xe000a000 mapped to 0xe080a000

    [    0.550000] SCSI subsystem initialized

    [    0.550000] usbcore: registered new interface driver usbfs

    [    0.560000] usbcore: registered new interface driver hub

    [    0.560000] usbcore: registered new device driver usb

    [    0.570000] Advanced Linux Sound Architecture Driver Version 1.0.24.

    [    0.570000] Switching to clocksource xttcpss_timer1

    [    0.590000] NET: Registered protocol family 2

    [    0.590000] IP route cache hash table entries: 4096 (order: 2, 16384 bytes)

    [    0.590000] TCP established hash table entries: 16384 (order: 5, 131072 bytes)

    [    0.600000] TCP bind hash table entries: 16384 (order: 5, 196608 bytes)

    [    0.600000] TCP: Hash tables configured (established 16384 bind 16384)

    [    0.610000] TCP reno registered

    [    0.610000] UDP hash table entries: 256 (order: 1, 8192 bytes)

    [    0.620000] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

    [    0.620000] NET: Registered protocol family 1

    [    0.630000] Trying to unpack rootfs image as initramfs...

    [    0.630000] rootfs image is not initramfs (no cpio magic); looks like an initrd

    [    0.670000] Freeing initrd memory: 8192K

    [    0.670000] xscugtimer xscugtimer.0: ioremap fe00c200 to e0810200 with size 400

    [    0.670000] pl330 dev 0 probe success

    [    0.680000] msgmni has been set to 972

    [    0.680000] io scheduler noop registered

    [    0.680000] io scheduler deadline registered

    [    0.680000] io scheduler cfq registered (default)

    [    0.690000] e00   0.690000] console [ttyPS0] enabled, bootconsole disabled
    [    0.690000] console [ttyPS0] enabled, bootconsole disabled

    [    0.700000] xdevcfg f8007000.devcfg: ioremap f8007000 to e0814000 with size 1000
    [    0.710000] [drm] Initialized drm 1.1.0 20060810
    [    0.720000] brd: module loaded
    [    0.730000] loop: module loaded
    [    0.730000] xqspips e000d000.qspi: at 0xE000D000 mapped to 0xE0816000, irq=51
    [    0.740000] GEM: BASEADDRESS hw: e000b000 virt: e0818000
    [    0.740000] XEMACPS mii bus: probed
    [    0.750000] mdio_bus c0197b60: error probing PHY at address 0
    [    0.750000] eth0, pdev->id -1, baseaddr 0xe000b000, irq 54
    [    0.760000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    [    0.760000] usb_hcd_xusbps_probe: No OTG assigned!
    [    0.770000] usb_hcd_xusbps_probe: OTG now assigned!
    [    0.770000] xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
    [    0.780000] xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
    [    0.810000] xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
    [    0.830000] xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
    [    0.830000] hub 1-0:1.0: USB hub found
    [    0.830000] hub 1-0:1.0: 1 port detected
    [    0.840000] Initializing USB Mass Storage driver...
    [    0.840000] usbcore: registered new interface driver usb-storage
    [    0.850000] USB Mass Storage support registered.
    [    0.850000] Xilinx PS USB Device Controller driver (Apr 01, 2011)
    [    0.860000] mousedev: PS/2 mouse device common for all mice
    [    0.860000] Linux video capture interface: v2.00
    [    0.870000] gspca_main: v2.14.0 registered
    [    0.870000] usbcore: registered new interface driver uvcvideo
    [    0.870000] USB Video Class driver (1.1.1)
    [    0.880000] WDT OF probe
    [    0.880000] xwdtps f8005000.swdt: Xilinx Watchdog Timer at 0xe081c000 with timeout 10 seconds
    [    0.890000] sdhci: Secure Digital Host Controller Interface driver
    [    0.890000] sdhci: Copyright(c) Pierre Ossman
    [    0.900000] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.900000] mmc0: Invalid maximum block size, assuming 512 bytes
    [    0.910000] mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
    [    0.920000] usbcore: registered new interface driver usbhid
    [    0.920000] usbhid: USB HID core driver
    [    0.930000] edid status: 1
    [    0.930000] adv7511 0-0039: Failed to add route DAI IN->TMDS
    [    0.950000] asoc: adv7511 <-> 75c00000.axi-spdif-tx mapping ok
    [    0.950000] axi-spdif 75c00000.axi-spdif-tx: Failed to set DAI format: -22
    [    0.960000] ALSA device list:
    [    0.960000]   #0: HDMI monitor
    [    0.970000] TCP cubic registered
    [    0.970000] NET: Registered protocol family 17
    [    0.970000] edid ret: 4
    [    0.980000] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    [    0.980000] Registering SWP/SWPB emulation handler
    [    0.990000] registered taskstats version 1
    [    0.990000] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
    [    0.990000] i2c ret: 2
    [    1.000000] mmc0: new high speed SDHC card at address b368
    [    1.000000] mmcblk0: mmc0:b368 SMI   3.69 GiB
    [    1.010000]  mmcblk0: p1
    [    1.010000] RAMDISK: gzip image found at block 0
    [    1.010000] i2c ret: 2
    [    1.020000] i2c ret: 2
    [    1.030000] i2c ret: 2
    [    1.030000] new mode: 1920x1080 2080x1111 138500
    [    1.030000] new mode: 1680x1050 2240x1089 146250
    [    1.040000] new mode: 1280x720 1650x750 74250
    [    1.040000] new mode: 1920x1080 2200x1125 74250
    [    1.050000] new mode: 720x480 858x525 27000
    [    1.050000] new mode: 720x480 858x525 27000
    [    1.050000] new mode: 1920x1080 2200x1125 148500
    [    1.060000] new mode: 1280x1024 1688x1066 108000
    [    1.060000] new mode: 1280x1024 1688x1066 135000
    [    1.060000] new mode: 1152x864 1520x895 81579
    [    1.070000] new mode: 1280x960 1728x1002 129936
    [    1.070000] new mode: 1152x864 1600x900 108000
    [    1.080000] new mode: 800x600 1056x628 40000
    [    1.080000] new mode: 640x480 840x500 31500
    [    1.080000] new mode: 640x480 800x525 25200
    [    1.090000] new mode: 720x400 900x449 28320
    [    1.090000] new mode: 1280x1024 1688x1066 135000
    [    1.090000] new mode: 1024x768 1312x800 78800
    [    1.100000] new mode: 1024x768 1328x806 75000
    [    1.100000] new mode: 1024x768 1344x806 65000
    [    1.100000] new mode: 832x624 1152x667 57284
    [    1.110000] new mode: 800x600 1056x625 49500
    [    1.110000] new mode: 1280x720 1650x750 74250
    [    1.110000] new mode: 1920x1080 2200x1125 74250
    [    1.120000] new mode: 720x480 858x525 27000
    [    1.120000] new mode: 720x480 858x525 27000
    [    1.120000] new mode: 1920x1080 2750x1125 74250
    [    1.130000] new mode: 1920x1080 2200x1125 74250
    [    1.130000] new mode: 1920x1080 2200x1125 148500
    [    1.140000] new mode: 720x576 864x625 27000
    [    1.140000] new mode: 1280x720 1980x750 74250
    [    1.140000] new mode: 720x576 864x625 27000
    [    1.150000] new mode: 1920x1080 2640x1125 74250
    [    1.150000] new mode: 1920x1080 2640x1125 148500
    [    1.150000] new mode: 1440x480 1716x525 27000
    [    1.160000] new mode: 1440x576 1728x625 27000
    [    1.180000] drivers/gpu/drm/analog/analog_drm_fbdev.c:analog_drm_fbdev_probe[241]
    [    1.180000] setting clock to: 138500
    [    1.180000] raw_edid: d816bac0 7
    [    1.180000] Using YCbCr output
    [    1.220000] Console: switching to colour frame buffer device 240x67
    [    1.260000] fb0:  frame buffer device
    [    1.260000] drm: registered panic notifier
    [    1.270000] [drm] Initialized analog_drm 1.0.0 20110530 on minor 0
    [    1.280000] EXT4-fs (ram0): warning: mounting unchecked fs, running e2fsck is recommended
    [    1.280000] EXT4-fs (ram0): mounted filesystem without journal. Opts: (null)
    [    1.290000] VFS: Mounted root (ext4 filesystem) on device 1:0.
    [    1.300000] Freeing init memory: 152K
    Starting rcS...
    ++ Mounting filesystem
    ++ Setting up mdev
    ++ Configure static IP 192.168.1.10
    [    1.480000] GEM: lp->tx_bd ffdfa000 lp->tx_bd_dma 18bd6000 lp->tx_skb d8ac39c0
    [    1.490000] GEM: lp->rx_bd ffdfb000 lp->rx_bd_dma 18bd5000 lp->rx_skb d8ac3ac0
    [    1.490000] GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
    [    1.500000] eth0: no PHY found
    [    1.500000] XEMACPS mii bus mii_probe fail.
    ifconfig: SIOCSIFFLAGS: No such device or address
    ++ Starting telnet daemon
    ++ Starting http daemon
    ++ Starting ftp daemon
    ++ Starting dropbear (ssh) daemon
    ++ Starting OLED Display
    [    1.550000] pmodoled-gpio-spi [zed_oled] SPI Probing
    ++ Exporting LEDs & SWs
    rcS Complete
    zynq>


    Cheers,

    - Bren