Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Baud Rate Xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 373 subscribers
  • Views 589 views
  • Users 0 members are here
Related

Baud Rate Xillinux

deaxman
deaxman over 13 years ago

Is baud rate hardware dependant for connecting to the UART or will it need to be changed now that I've started using Xillinux instead of the default installation of linux?  I am only getting gibberish in the terminal when I try to connect with the 115200 baud rate and 10, 100 delay times for the serial connection. Is the baud rate different now?  I can't find any documentation on connecting with the UART to Xillinux, it just says it's only used rarely.  Thanks!!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    That's a common situation when turning the board off and on with the terminal application running. The USB interface vanishes, and then a new one is generated when the board goes on again. The terminal remains connected to a stale UART of USB instance. So nothing happens.

       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    That's a common situation when turning the board off and on with the terminal application running. The USB interface vanishes, and then a new one is generated when the board goes on again. The terminal remains connected to a stale UART of USB instance. So nothing happens.

       Eli