Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Stuck on Xillinux Tutorials
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 372 subscribers
  • Views 370 views
  • Users 0 members are here
Related

Stuck on Xillinux Tutorials

icebryanchan
icebryanchan over 9 years ago

Hi,
I just got my Zedboard and I am planning to do a FPGA coprocessing project on it. 
I followed the tutorials given and everything went smoothly until Part V.
http://xillybus.com/tutorials/vivado-hls-c-fpga-howto-5
 
Before applying the given HLS sample code, I am able to send and receive data to and from the FIFO.
However, after generating the new bitstream file from the sample code, the FIFO is not working on both 8-bit and 32-bit.
I have read the tutorial over and over and I realize I have to generate a new boot.bin file according to the bitfile generated.
QUOTING:

 

Using the bitfile
The bitfile is used as before, when the plain Xillybus bundle was implemented. For PCIe-based platforms, the bitfile is loaded through JTAG to the FPGA (note that the host should be turned off while this is done). If Zedboard is targeted, a new boot.bin file should be generated, based upon the new bitfile, and copied to the SD card like before.
 
 
So the problem is that I can't seem to find any tutorial on how to generate boot.bin file from the freshly generated bitfile.

 

Can anyone help me on this? Just a link or a tutorial will be good for me. Any help would be appreciated very much. Thanks in advanced.
 
Thanks and best regards.

 

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Bryan,

    Please ask this question to the creators of the material.

    Or ask over at Digilent as they are the main point of contact for educational support

    Thanks,

    Josh