Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General microblaze on Zedboard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 372 subscribers
  • Views 698 views
  • Users 0 members are here
Related

microblaze on Zedboard

fayyazrafiq
fayyazrafiq over 13 years ago

I am facing problem to have microblaze on Zedboard alongwith ARM PS. I use the same design which was given on AR#50869(http://www.xilinx.com/support
/answers/50869.html#linkedARRecords)
and change the board specification in XPS Graphical view/import. Then I generate bit stream named system.bit. Then I follow the same procedure given in AR#50869 to download and create an image. I copy the image on the SD card (Boot.bin). I setup the jumpers on the ZedBoard for booting from SD card. Noting happenu2026 After that I open the XMD Console, I write on the command prompt
u201Cconnect mb mdmu201D. After that I got an error, no mdm found. Please help meu2026.
I shall very grateful for any help.
Fayyaz

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 13 years ago

    Well, just looking at this error message, it is saying you tried to synthesize 2.4 GHz for FVCO on an MMCM, and that is not allowed. That doesn't seem to match with your statement regarding your changes related to enabling PS GPIO through the EMIO. Besides adding GPIO to EMIO, did you change anything else? If you can provide more details on what project you started with and what you changed, that will help us re-trace your steps.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 13 years ago

    Well, just looking at this error message, it is saying you tried to synthesize 2.4 GHz for FVCO on an MMCM, and that is not allowed. That doesn't seem to match with your statement regarding your changes related to enabling PS GPIO through the EMIO. Besides adding GPIO to EMIO, did you change anything else? If you can provide more details on what project you started with and what you changed, that will help us re-trace your steps.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fayyazrafiq
    0 fayyazrafiq over 13 years ago in reply to bhfletcher

    Dear
    Thank you again for the reply. Actually, I started with the project given with AR#50869 (http://www.xilinx.com/support/answers/50869.html). I only made connection for GPIO to EMIO. Actually, I solve the problem by changing the Clock_generator_0 input frequency to 100 MHz. Previously, it was 50 MHz. Now I have the same input (100 MHz) and output (100 MHz) frequency. I generate the bit stream, it is ok. I also tested the code on the arm processor. I am able to flash the LED0 on the ZedBoard. I observed a strange behaviour, the flashing of LED is very slow. Although, I set the blinking time to 1 tick interval.
    Could you please explain, is there anything wrong? Do, I need to change the Clock_Generator_0 setting to something else.

    Any help is highly appreciated.
    Thanks
    Fayyaz