Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ZedBoard MAC Address
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 373 subscribers
  • Views 1791 views
  • Users 0 members are here
Related

ZedBoard MAC Address

100alexj
100alexj over 8 years ago

Hi,

 

Where can I find the MAC address of my ZedBoard? I need the MAC address so that I can store it into my networks DHCP lookup table. Does a certain piece of code need to be running in order for the board to receive a MAC address? The board is right now connect to my network via an Ethernet cable.

 

Any help will be greatly appreciated. 

 

Thank you,

-Alex

  • Sign in to reply
  • Cancel
Parents
  • 100alexj
    0 100alexj over 8 years ago

    Sorry to open this back up, but I still have a few questions.

     

    When I plug in the SD card that comes with the ZedBoard and run the code in PuTTY I notice the MAC address is 00:0A:35:00:01:22. When the SD card is not plugged in I am assuming the ZedBoard does not have a MAC address. Is my assumption correct? Is there a way to assign a permanent MAC address to the board to where it stays the same upon reset and without the SD card?

     

    FYI I am using a windows machine and currently do not have access to Linux.

     

    Thank you,

     

    -Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100alexj
    0 100alexj over 8 years ago

    Sorry to open this back up, but I still have a few questions.

     

    When I plug in the SD card that comes with the ZedBoard and run the code in PuTTY I notice the MAC address is 00:0A:35:00:01:22. When the SD card is not plugged in I am assuming the ZedBoard does not have a MAC address. Is my assumption correct? Is there a way to assign a permanent MAC address to the board to where it stays the same upon reset and without the SD card?

     

    FYI I am using a windows machine and currently do not have access to Linux.

     

    Thank you,

     

    -Alex