Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zedboard PS iic setup
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 373 subscribers
  • Views 1502 views
  • Users 0 members are here
  • ZedBoard General Questions
  • adv7511
  • Software Application Development
  • zedboard_questions
  • iic
Related

Zedboard PS iic setup

tconlon03
tconlon03 over 7 years ago

Hi guys,

 

I'm trying to configure the ADV7511 chip for HDMI output on the zedboard but running into trouble with iic. I have configured device XPAR_XIICPS_0_DEVICE_ID/XPAR_PS7_I2C_0_DEVICE_ID without any issues however when i attempt to do any operation that uses XIicPs_MasterSendPolled the program hangs. I've included an example below where im reading from the HPD State register(0x42) of the ADV7511(iic address - 0x39).

 

// Set the address of the register to read

Status = XIicPs_MasterSendPolled(IicPs, &Register, 1, Address);

 

****Variable values at time of call

image

 

 

**Hangs here

/*

* Check for completion of transfer.

*/

while ((IntrStatusReg & XIICPS_IXR_COMP_MASK) != XIICPS_IXR_COMP_MASK){

 

 

IntrStatusReg = XIicPs_ReadReg(BaseAddr, XIICPS_ISR_OFFSET);

/*

* If there is an error, tell the caller.

*/

if ((IntrStatusReg & Intrs) != 0U) {

return (s32)XST_FAILURE;

}

}

 

 

The zedboard has the same zynq soc as the ZC702 board (Zynq-7000 XC7Z020-1CLG484C SoC) so i thought maybe i had to set a iic mux at address 0x74 as shown in the ZC702 user guide however this also hangs.

Hopefully someone can explain why the PS iic isnt working properly

 

Thanks!

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi,

    Are you able to use the PL IIC controller? We have found much more success with that in the past. If not, why so?

     

    Thanks,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • tconlon03
    0 tconlon03 over 7 years ago in reply to jafoste4

    Hi,

     

    That is what I am attempting at the minute. The PS implementation made more sense to me and was wondering why it wasnt working.