Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General PicoZed USB PHY always in RESET?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 372 subscribers
  • Views 1103 views
  • Users 0 members are here
  • reset
  • PicoZed Hardware Design
  • usb_phys
Related

PicoZed USB PHY always in RESET?

400garrison
400garrison over 7 years ago

We have an issue in which the USB PHY (USB3320) is always held in RESET.  The attached picture describes the issue also.

image

The root cause is the following:

  1. PS_MIO7 signal is 1.8V due Bank 501 being set to 1.8V.
  2. TI AND gate IC SN74AUP2G08DQER is spec'd VIH = 2V min

  3. Therefore the input to the AND logic can never = 1 (>2V).
  4. Therefore the signal USB_OTG_RST_N.

 

This design is across the Rev A, C, and E schematics.  How can we ensure that the USB3320 device is not in reset.

 

Thank you,

 

Adam

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 7 years ago +1 suggested
    Hi Adam, Refering to the schematic for the PicoZed 7010/7020 or PicoZed 7015/7030 SOM, PS_MIO7 is tied to Bank 500. 3005.contentimage_189921.png and bank 500 is driven to 3.3V. 3821.contentimage_189922…
Parents
  • jafoste4
    0 jafoste4 over 7 years ago

    Hi Adam,

     

    Refering to the schematic for the PicoZed 7010/7020 or PicoZed 7015/7030 SOM, PS_MIO7 is tied to Bank 500.

    3005.contentimage_189921.png

     

    and bank 500 is driven to 3.3V.

    3821.contentimage_189922.png

     

    let me know if you need any further explanation.

     

    Thanks!

    Josh

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to jafoste4

    Which is what I just told him .

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 7 years ago in reply to jafoste4

    Which is what I just told him .

     

    MK