Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General PicoZed Bank13 IO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 374 subscribers
  • Views 1034 views
  • Users 0 members are here
  • ZedBoard General Questions
  • PicoZed Hardware Design
Related

PicoZed Bank13 IO

ivarhl
ivarhl over 7 years ago

Hello.

I have just designed a carrier board for a PicoZed 7015/7030. I have verified all power and boot up, and it works, now I want to use the FPGA and the IOs.

 

I have been able to access the IOs of bank 34/35, and this works fine. I have also been able to use the MIO pins. But I have an issue when it comes to the IO pins of Bank 13. I have not been able to use those yet. I have tried connecting them diretly to PL like I did with bank 34/35, e.g. by setting a counter in PL and connecting IO's directly to the output of the counter. I have also tried accessing this from PS via EMIO. But I cannot seem to get these pins to change...

 

Is there any setting in Vivado that needs to be set? When I tried EMIO i enable EMIO and used a constraint file to set the pins. When I tried directly form PL I used the same method that worked for bank 34/35, and this is to set the IOs via contraint file. I have only tried these as outputs yet.

 

Any tips?

  • Sign in to reply
  • Cancel

Top Replies

  • ivarhl
    ivarhl over 7 years ago in reply to jafoste4 +1
    Joshua, I will see if can get a hold of one Avnet carrier board. Unfortunately I cannot share schematics, since this is work related, such information is not allowed to share...
  • ivarhl
    ivarhl over 6 years ago +1
    I found the error, it was a HW error, probbably a loose connection (bad soldering etc) in the board to board connector. Problem solved.
Parents
  • clem57
    0 clem57 over 7 years ago

    ivarhl  wrote:

     

    Hello.

    I have just designed a carrier board for a PicoZed 7015/7030. I have verified all power and boot up, and it works, now I want to use the FPGA and the IOs.

     

    I have been able to access the IOs of bank 34/35, and this works fine. I have also been able to use the MIO pins. But I have an issue when it comes to the IO pins of Bank 13. I have not been able to use those yet. I have tried connecting them diretly to PL like I did with bank 34/35, e.g. by setting a counter in PL and connecting IO's directly to the output of the counter. I have also tried accessing this from PS via EMIO. But I cannot seem to get these pins to change...

     

    Is there any setting in Vivado that needs to be set? When I tried EMIO i enable EMIO and used a constraint file to set the pins. When I tried directly form PL I used the same method that worked for bank 34/35, and this is to set the IOs via contraint file. I have only tried these as outputs yet.

     

    Any tips?

    The only difference I see is the 34/35 are power from carrier card and have voltage you set. On the other hand 13 is powered by zed-board and are fixed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ivarhl
    0 ivarhl over 7 years ago in reply to clem57

    Bank 13 is powered from the carrier, JX2 pin 98 and JX3 pin 45 and 46. I also see no other difference. Could there be some settings in Vivado I have missed or set incorrectly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ivarhl
    0 ivarhl over 7 years ago in reply to clem57

    Bank 13 is powered from the carrier, JX2 pin 98 and JX3 pin 45 and 46. I also see no other difference. Could there be some settings in Vivado I have missed or set incorrectly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jafoste4
    0 jafoste4 over 7 years ago in reply to ivarhl

    HI Ivar,

     

    Try making the same design on one of the Avnet Carrier Cards to verify your process in accessing that bank.

    ALso are you interested in sharing your schematics?

     

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ivarhl
    0 ivarhl over 7 years ago in reply to jafoste4

    Joshua,

     

    I will see if can get a hold of one Avnet carrier board.

     

    Unfortunately I cannot share schematics, since this is work related, such information is not allowed to share...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 7 years ago in reply to ivarhl

    Hi Ivar,

     

    I understand! You may want to reach out to one of your local Avnet FAEs for assitance as well.

     

    -Josh