Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Can I use AFE7444EVM (JESD204B) with PicoZed FMC Carrier V2?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 373 subscribers
  • Views 1063 views
  • Users 0 members are here
  • ZedBoard General Questions
  • picozed
  • PicoZed Hardware Design
  • Zedboard Training
Related

Can I use AFE7444EVM (JESD204B) with PicoZed FMC Carrier V2?

rforti
rforti over 6 years ago

Hi,

 

I am currently developing a new application where I need to measure the FFT of three signals that contain multiple frequency components (between 50 and 400 MHz). My initial plan was to use an ADC evaluation module from Texas Instruments (AFE7444EVM), together with the 7015 PicoZed and the PicoZed FMC Carrier Card V2 (I would rather not develop a carrier card myself).

 

I have three questions about this implementation:

 

1- Can I directly connect the FMC connectro from AFE7444EVM to the PicoZed Carrier card (i.e., is the PicoZed FMC Carrier Card compatible with the JESD204B IP)?

2- Can I do the FFT analysis directly in the PicoZed or should I transfer the data to a PC? What do you think would be the faster option (I only need the AC power and phase of specific frequencies)?

3- Is the 7015 PicoZed fast enough for my application? Or should I use another board?

 

PS1: If you need any extra information about my system design, please let me know.

PS2: I am very new to FPGA development, so detailed answers or any good references are very welcomed.

  • Sign in to reply
  • Cancel
Parents
  • mbrown
    0 mbrown over 6 years ago

    Hi Rodrigo,

     

    I have a few ideas, but knowing your end goal will help me suggest something relevant.

     

    Is your final goal to put something into production using the PicoZed module, or is this system an academic/R&D type project?

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mbrown
    0 mbrown over 6 years ago

    Hi Rodrigo,

     

    I have a few ideas, but knowing your end goal will help me suggest something relevant.

     

    Is your final goal to put something into production using the PicoZed module, or is this system an academic/R&D type project?

     

    /Matt

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rforti
    0 rforti over 6 years ago in reply to mbrown

    Hi Matt,

    Thanks so much for the fast response!!

    This is an academic project. That's also one of the reason why I don't want to develop my own carrier boards, as it would take much longer to have a working prototype of the final system. Please let me know if you need extra information!