Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General I have a problem setting the USB3 in UltraZed-3EG
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 803 views
  • Users 0 members are here
  • ZedBoard General Questions
  • Ultrazed Hardware Design
  • zedboardcmty
Related

I have a problem setting the USB3 in UltraZed-3EG

sint12345
sint12345 over 6 years ago

Hi,

 

How I am defining through PetaLinux (2018.3) the USB3 of the UltraZed-EG, as apparently it doesn’t support the previous setup ( of Ultra96-V1 and V2).

 

The main command ifconfig usb0 192.168.100.1 netmask 255.255.255.0  and modprobe g_ether

 

Are not recognized in UltraZed-3EG as they were recognized in Ultra96-v1 or v2.

 

I am getting the following messages:

 

479.877751] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[ 481.965750] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[ 484.053749] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[ 486.141749] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[ 488.229748] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

[ 490.317748] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?

 

I have replaced two cables that works well in Ultr96-V2 Boards and got the same messages.

 

Why it specifies USB2 and not USB3, is the connector of J15 shouldn’t be 2-3?

 

 

What should be the mode of ID J15, currently it connected 2-3 I am looking at four jumpers that refers to USB modes: power and ID,

 

They look okay they are in configuration of host not otg and not device.

 

 

Thanks,

 

Shiri

  • Sign in to reply
  • Cancel
Parents
  • sint12345
    0 sint12345 over 6 years ago

    Thanks for your answer, although I have replaced the cable, and I used the same cables that worked great at Ultra96V2 with no problem.

     

    I do think the main problem is that the driver of g_ether was not loaded properly as it is not recognized.

     

    I think because the bsps may be different than the driver was not loaded properly

     

     

    modprobe g_ether -

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sint12345
    0 sint12345 over 6 years ago

    Thanks for your answer, although I have replaced the cable, and I used the same cables that worked great at Ultra96V2 with no problem.

     

    I do think the main problem is that the driver of g_ether was not loaded properly as it is not recognized.

     

    I think because the bsps may be different than the driver was not loaded properly

     

     

    modprobe g_ether -