Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General UltraZed-EV & SDAccel 2019.1
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 839 views
  • Users 0 members are here
  • Using Xilinx Tools
  • Ultrazed Hardware Design
  • zedboardcmty
Related

UltraZed-EV & SDAccel 2019.1

gdufourcq
gdufourcq over 6 years ago

Hi,

I've downloaded the UltraZed-Ev platform file from here:

http://zedboard.org/support/design/25481/161

 

and I ran a synthesis with SDAccel 2019.1 on one of the Xilinx SDAccel example design and I faced the following issue:

WARNING: [Vivado 12-508] No pins matched '/zynq_ultra_ps_e_0_pl_clk0'.

INFO: [Timing 38-35] Done setting XDC timing constraints.

WARNING: [Vivado 12-1008] No clocks found for command 'get_clocks -of_objects [get_pins /zynq_ultra_ps_e_0_pl_clk0]'.

Resolution: Verify the create_clock command was called to create the clock object before it is referenced.

INFO: [Vivado 12-626] No clocks found. Please use 'create_clock' or 'create_generated_clock' command to create clocks.

ERROR: [runtcl-1] ERROR: [Common 17-55] 'get_property' expects at least one object.

Resolution: If [get_<value>] was used to populate the object, check to make sure this command returns at least one valid object.

ERROR: [Common 17-39] 'send_msg_id' failed due to earlier errors.

 

Is there an issue with the UltraZed-EV platform file?

I've also tested with the Vitis 2020.1 and got the exact same issue

 

Regards

  • Sign in to reply
  • Cancel

Top Replies

  • drozwood90
    drozwood90 over 6 years ago +1 verified
    Hi there, The platform you linked above was designed to be run with SDSoC 2019.1 only. SDAccel does not support SoC chips. It is designed to use a more PURE FPGA configuration. If you wish to run with…
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    The platform you linked above was designed to be run with SDSoC 2019.1 only.  SDAccel does not support SoC chips.  It is designed to use a more PURE FPGA configuration.

     

    If you wish to run with Vitis, we have a Vitis platform ready for download with a prebuilt example application located on the UltraZed-EV Resourcing page.

    UltraZed-EV

    1401.contentimage_191949.png

    --Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • gdufourcq
    0 gdufourcq over 6 years ago in reply to drozwood90

    Hi Daniel,

    I've tested with the Vitis platform you suggested and it worked fine.

    Thanks for your help!