Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General ultra96 v2 board pynq overlay problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 373 subscribers
  • Views 1335 views
  • Users 0 members are here
  • Using Xilinx Tools
  • Software Application Development
  • Ultra96 Hardware Design
  • zedboardcmty
Related

ultra96 v2 board pynq overlay problem

tim7107
tim7107 over 6 years ago

Hello everyone, I am new to pynq ultra96 v2 board. I am going to create a custom about matrix multiplication or simple calculation using Vivado HLS with C or C++.

But i meet some problem about what data type to use in order to feed the  input array into the void function in Vivado HLS.

And I also do not know how to write the code about hardware port such as s_axilite or something else and then return the output array so that i can call the function on jupyter using python?

It would be grateful that if someone can give me some tutorial or project or advices!!

Thanks a lot!

Tim

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 6 years ago

    Hi there,

     

    You can also take a look at this:

    https://github.com/twaclaw/matmult

     

    Seems to be exactly what you wanted.  PYNQ being as open and community involved, there is a LOT of material that you can locate with a few online searches.  Especially since Pynq's target is to be as open and ready to be leveraged!

    You can also take a look at the Hackster.IO course that we have which teaches PYNQ.

    Check out "Turbocharge Python with Ultra96 PYNQ"

    https://www.hackster.io/workshops/ultra96#page-block-k9zmaswy9j

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim7107
    0 tim7107 over 6 years ago in reply to drozwood90

    Hi Daniel Rozwood,

    Thanks for your help!!

    I have seen that version on github before but i can not connect the matrix ip and the board system successful.

    I do not knom why. Could it be the problem that the board vision is not pynq z1 so that the ip can not be connected in vivado?

    And i have chosen the port to the ultra96 v2 board port when creating C code using vivado hls.

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • drozwood90
    0 drozwood90 over 6 years ago in reply to tim7107

    Hi there,

     

    With the correct hooks in place, there should be no issue with the IP going between system to system.

    I would suggest that training I pointed out.  That only takes 1-2 days and you can go at your own pace.

     

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 6 years ago in reply to tim7107

    Hi there,

     

    With the correct hooks in place, there should be no issue with the IP going between system to system.

    I would suggest that training I pointed out.  That only takes 1-2 days and you can go at your own pace.

     

    --Dan