Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Maximum frequency inputs of Zedboard PMODs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 373 subscribers
  • Views 2805 views
  • Users 0 members are here
  • ZedBoard General Questions
  • Zedboard Hardware Design
  • Zedboard Training
  • zedboardcmty
Related

Maximum frequency inputs of Zedboard PMODs

longgang
longgang over 5 years ago

Hi, I am new to the Zedboard. I want to use an ADC with SPI 5MHZ throughout, which means SDO will reach to around 100MHZ  with 16bits. Then, I want to use PMODS JA-JD to receive the data from the ADC. What worries me is that could Zedboard PMOD pins are available to receive such inputs with 100 Mhz?  I know the I/O banks of FPGA in the PL side can reach 2-4 times of the main clock, but here the problem is the path from Zedboard Pmod pins to the PL GPIO blocks.

 

Could someone help me? Thanks so much!!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago +1
    What ADC are you planning to use ? You need to look very carefully at the timing margins - frequently ADCs have "keep out " times which will push the clock frequency up and may not work well with standard…
  • drozwood90
    drozwood90 over 5 years ago +1 verified
    Hi there, On Zedboard, the limit is going to come up in the connector. It is not a high speed connector. A quick Google search and you should be able to locate the PMOD specification. It is maintained…
  • longgang
    longgang over 5 years ago in reply to drozwood90 +1 suggested
    Hi Dan, Thanks for the reply. I think this is what I am looking for. I read through the hardware user guider of Zedboard. It only mentions that the JC1 and JD1 support 525Mhz LVDS, but no information about…
Parents
  • drozwood90
    0 drozwood90 over 5 years ago

    Hi there,

     

    On Zedboard, the limit is going to come up in the connector.  It is not a high speed connector.

    A quick Google search and you should be able to locate the PMOD specification.  It is maintained by Digilent.

    https://reference.digilentinc.com/_media/reference/pmod/digilent-pmod-interface-specification.pdf

    According to that:
    "The Pmod interface is not intended for high frequency operation, however, using RJ45 connectors and twisted pair Ethernet cable, signals have been sent reliably at 24Mhz and distances of up to 4 meters."

    If you are careful, you can probably go higher, but you will need to check with Samtec as well as determine the constraint for the SI related to the board trace lengths and package delays - as you will start hitting SI issues.  On Avnet created boards, we have hit speeds in the low 100's of MHz, but that was using special cables, routed boards, etc. on PIcoZed.  I cannot say that the Digilent routed board would operate at those speeds.

     

    If you really want high speed, use the FMC.  That is why it is there.  The Vita57 spec calls out "signaling speed of 2 Gbps" for the IO and much higher for transceivers.  I do not believe the ZedBoard has transceivers, but I think 2Gbps far exceeds what you are calling out.

     

    --Dan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • longgang
    0 longgang over 5 years ago in reply to drozwood90

    Hi Dan,

     

    Thanks for the reply.

    I think this is what I am looking for. I read through the hardware user guider of Zedboard. It only mentions that the JC1 and JD1 support 525Mhz LVDS, but no information about JA and JB. Since I want to use all the Pomds on the zedboard around 100MHZ for multi-channel ADC/DAC,  JA and JB really confused me. I think I need to create a PCB design with an FMC adaptor to achieve my applications.

     

    Longgang

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • longgang
    0 longgang over 5 years ago in reply to drozwood90

    Hi Dan,

     

    Thanks for the reply.

    I think this is what I am looking for. I read through the hardware user guider of Zedboard. It only mentions that the JC1 and JD1 support 525Mhz LVDS, but no information about JA and JB. Since I want to use all the Pomds on the zedboard around 100MHZ for multi-channel ADC/DAC,  JA and JB really confused me. I think I need to create a PCB design with an FMC adaptor to achieve my applications.

     

    Longgang

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer