Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General u-boot fpga loadb issues on Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 371 subscribers
  • Views 942 views
  • Users 0 members are here
  • ZedBoard General Questions
  • zedboardcmty
Related

u-boot fpga loadb issues on Microzed

rdb98789
rdb98789 over 5 years ago

A long time ago, I had written in my notes that I could load the FPGA bitstream via TFTP from the u-boot terminal using these commands:

 

> tftpboot 0x4000000 192.168.8.20:top.bit

> fpga loadb 0 0x4000000 0x${filesize}

 

Now when I try this, it looks like it is starting to work properly (it prints information about the FPGA, the version of Vivado, the user ID, build date, etc), but it never really finishes. It instead shows:

 

"Usage:

fpga [operation type] [device number] [image address] [image size]

..."

 

And the configuration LED doesn't turn on, and my expected blinky LEDs don't blinky.

 

This sequence of commands works fine on the zc706, as I just tested it, but I can't seem to get it to work on the Microzed (even though I have in my notes that it used to work).

The fpga part number for the bitstream matches my target device.

 

Is there a trick to getting this command to work?

  • Sign in to reply
  • Cancel
Parents
  • rdb98789
    0 rdb98789 over 5 years ago

    Also, this is running the default version of u-boot that comes pre-installed on the QSPI flash.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rdb98789
    0 rdb98789 over 5 years ago

    Also, this is running the default version of u-boot that comes pre-installed on the QSPI flash.