Avnet Boards Forums
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General MicroZed SD Card boot problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 373 subscribers
  • Views 1556 views
  • Users 0 members are here
  • MicroZed Hardware Design
  • zedboardcmty
Related

MicroZed SD Card boot problem

hixboz
hixboz over 4 years ago

Hello all,

 

I am trying to build custom Linux for MicroZed 7010 by using Petalinux 2018.3. I would like to boot it from sd card. I have installed Petalinux and I have only changed INITRAMFS mode to SD card mode from "petalinux-config" . Than I have compiled the system without any error. My sd card is SDHC 16GB class 10. I have formatted it with two partitions as vfat and ext4. After compilation process has done, I copied to BOOT.BIN and image.ub file to first partition. For rootfs, I used the command like "sudo dd if=rootfs.ext4 of=/dev/sdb2 conv=fsync bs=1M".

 

I got below message and booting process has stopped before root login.

"bootconsole [earlycon] disabled"

 

In u-boot, I have changed the bootargs as

"earlycon console=ttyPS1,115200"

 

After that, I got lastly this message and I couldn't get into root login.

"Starting tcf-agent: OK"

 

I have set the boot jumpers correctly. How can I solve this problem?

Thanks inadvanced. 

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    jafoste4 over 4 years ago

    Hi,

     

    Just to confirm using one of our pre-built images are you able to boot your MicroZed?

    Verifying this would validate your jumper settings and the quality of your SD Card. Leaving the only variable to look into being your custom image.

     

    Also when you built your image were you starting from one of our petalinux BSPs?

     

    Thx,

    Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • hixboz
    hixboz over 4 years ago in reply to jafoste4

    Hello Josh,

     

    I noticed that there is no "primary sd" option under "Advanced bootable images storage media->boot image settings" while configuration process. I checked the tutorials which explains booting from sd card and there is "primary sd" option in these tutorials. I got lastly  "Starting tcf-agent:OK" message and there is no any error. In tutorials, root login prompt comes after "Starting tcf-agent:OK" message. I suspect that the root filesystem configurations. Additionally, I observerd the root file system typing "ls mmc 0:2" in u-boot. Is there a chance that root filesytem not mounting from sd card to system?

     

    Thanks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hixboz
    hixboz over 4 years ago in reply to jafoste4

    Hello Josh,

     

    I noticed that there is no "primary sd" option under "Advanced bootable images storage media->boot image settings" while configuration process. I checked the tutorials which explains booting from sd card and there is "primary sd" option in these tutorials. I got lastly  "Starting tcf-agent:OK" message and there is no any error. In tutorials, root login prompt comes after "Starting tcf-agent:OK" message. I suspect that the root filesystem configurations. Additionally, I observerd the root file system typing "ls mmc 0:2" in u-boot. Is there a chance that root filesytem not mounting from sd card to system?

     

    Thanks.