Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Avnet Boards General Zynq Ultrascale+ Boards with FMC Imageon
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 372 subscribers
  • Views 1179 views
  • Users 0 members are here
  • fmc
  • imageon
  • ultrascale+
Related

Zynq Ultrascale+ Boards with FMC Imageon

BOK
BOK over 4 years ago

Hello, 

I'm using Ultrascale board based xczu9eg chip and also want to using FMC-IMAGEON card.

Since the reference design of fmc-imageon only consists of zynq-7000, the design has been changed as follows.

I changed the pin constraint related to the FMC signal, and tried to operate the board and the FMC card through the Vitis files that run HDMI-passthrough.

Then I can check this result.

imageimage

If FMC-IMAGEON is operating normally, I think that the HDMI source from PC should be output to the monitor.

But nothing display on monitor.

Is it impossible to using FMC-IMAGEON on UltraScale Boards?

or Any suggestions please.

Regards,

P.S.

On the FMC connector side and the pin setting of ADV7X11, I found that ZYNQ is LVCMOS25 and UltraScale is LVCMOS18. Could this part be causing the problem?

  • Sign in to reply
  • Cancel
  • nikltp
    0 nikltp over 3 years ago

     Are there any support teams on this forum? I do not see any reply. 

     BOK , Were you able to solve the issue? 

    I am also facing exactly the same type of issue. I am carrying out a test on the zcu102 board using the 2021 xilinx tool version. I have followed this git link for the IP and Source Code.

    https://github.com/Avnet/hdl/tree/master/Projects/fmchc_python1300c/software/fmchc_python1300c_app/src

    Everything seemed to be fine. I did not get any issues while programming.  The programming was also successful as I was able to read back all the programmed register values. However, there was no output. The same type of design works on Zedboard. 

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to nikltp

    "On the FMC connector side and the pin setting of ADV7X11, I found that ZYNQ is LVCMOS25 and UltraScale is LVCMOS18. Could this part be causing the problem?"

    Are you saying that the Zync board that you're using is interfacing with I/O bank set to a different voltage than the IMAGEON board? If so, then yes, that would be a big problem.

    There may be other issues, but I can't help, I can't even find a schematic for the board. However, that comment above was an important thing that stood out.